cancel
Showing results for 
Search instead for 
Did you mean: 

STM32CubeProgrammer 2.18 BUG on STM32H730

COSEBE
Senior

Hi,

I found a bug on new version 2.18 STM32Cube programmer.

Of course, I have the same problem with the new version of STM32CubeIde 1.17

It looks file STM32_Prog_DB_0x483.xml in \Data_Base folder has changed between versions 2.17 and 2.18

If I use the file STM32_Prog_DB_0x483.xml from the version 2.17 and I replace this file in version 2.18, I can access my STM32H730 device.

We tried it on 2 different computers.

I do not really understand the xml file differences, so I do not know if I can continue to use STM32_Prog_DB_0x483.xml file of version 2.17 with version 2.18 and STM32CubeIDE 1.17

Do you have a workaround ?

Sébastien

2 REPLIES 2
Maryem
ST Employee

Hello @COSEBE,

 

Thank you for reaching out.

To better understand and assist you with the problem, could you please provide more details on the specific issue you are experiencing?

 

Maryem.


In order to give better visibility on the answered topics, please click on 'Accept as Solution' on the reply which solved your issue or answered your question.

Hi,

this is the message I get when I want to connect to my device

(you have the Device ID at the bottom right)

COSEBE_0-1734682856971.png

This is the message I got when I want programming

COSEBE_1-1734682949161.png

This is on version 2.18

When I replace the XML file from version 2.17 in version 2.18, no more problem

 

Sébastien