cancel
Showing results for 
Search instead for 
Did you mean: 

STM32CubeProgrammer 2.18 BUG on STM32H730

COSEBE
Senior

Hi,

I found a bug on new version 2.18 STM32Cube programmer.

Of course, I have the same problem with the new version of STM32CubeIde 1.17

It looks file STM32_Prog_DB_0x483.xml in \Data_Base folder has changed between versions 2.17 and 2.18

If I use the file STM32_Prog_DB_0x483.xml from the version 2.17 and I replace this file in version 2.18, I can access my STM32H730 device.

We tried it on 2 different computers.

I do not really understand the xml file differences, so I do not know if I can continue to use STM32_Prog_DB_0x483.xml file of version 2.17 with version 2.18 and STM32CubeIDE 1.17

Do you have a workaround ?

Sébastien

10 REPLIES 10
Maryem
ST Employee

Hello @COSEBE,

 

Thank you for reaching out.

To better understand and assist you with the problem, could you please provide more details on the specific issue you are experiencing?

 

Maryem.


In order to give better visibility on the answered topics, please click on 'Accept as Solution' on the reply which solved your issue or answered your question.

Hi,

this is the message I get when I want to connect to my device

(you have the Device ID at the bottom right)

COSEBE_0-1734682856971.png

This is the message I got when I want programming

COSEBE_1-1734682949161.png

This is on version 2.18

When I replace the XML file from version 2.17 in version 2.18, no more problem

 

Sébastien

Hello @COSEBE ,

 

Thank you for your feedback.

I tried connecting an STM32H735 (same Device ID 0x483) and downloading a firmware using version 2.18.0 but couldn't reproduce the issues.

Maryem_0-1734687078571.png

Could you please also provide your option bytes configuration? Thank you in advance !

 

Maryem.


In order to give better visibility on the answered topics, please click on 'Accept as Solution' on the reply which solved your issue or answered your question.

You do not use the same device. 

Same ID, Yes, but not the same.

Can you check the XML file of ID 483.

Why when I change it, it works. My customer has exactly same problem

Sébastien

Value Series part, less/minimal FLASH tested/encoded in part..

Please try exact part as OP

Tips, Buy me a coffee, or three.. PayPal Venmo
Up vote any posts that you find helpful, it shows what's working..

I apologize for the oversight. I focused on the Device ID primarily, as I did not have the exact part number on hand at the moment. I will try to obtain it and test with it. I'll update you shortly.

 

Maryem.


In order to give better visibility on the answered topics, please click on 'Accept as Solution' on the reply which solved your issue or answered your question.

Any update on this problem ? 

Did you analyse XML file ?

 

Sébastien 

COSEBE
Senior

Can someone from ST team check the XML file and find a safe workaround ?

Regards,

Sebastien

Hello,

 

I've submitted an internal ticket for our dev team to address this issue,

Internal ticket number: 199559 (This is an internal tracking number and is not accessible or usable by customers)

I will keep you updated about any progress.

 

Maryem.


In order to give better visibility on the answered topics, please click on 'Accept as Solution' on the reply which solved your issue or answered your question.