2024-12-19 2:03 PM
Hi,
I found a bug on new version 2.18 STM32Cube programmer.
Of course, I have the same problem with the new version of STM32CubeIde 1.17
It looks file STM32_Prog_DB_0x483.xml in \Data_Base folder has changed between versions 2.17 and 2.18
If I use the file STM32_Prog_DB_0x483.xml from the version 2.17 and I replace this file in version 2.18, I can access my STM32H730 device.
We tried it on 2 different computers.
I do not really understand the xml file differences, so I do not know if I can continue to use STM32_Prog_DB_0x483.xml file of version 2.17 with version 2.18 and STM32CubeIDE 1.17
Do you have a workaround ?
Sébastien
Solved! Go to Solution.
2025-01-20 7:57 AM
Hello @COSEBE ,
I've sent you a message. Could you check your DM?
Maryem.
2024-12-19 11:59 PM
Hello @COSEBE,
Thank you for reaching out.
To better understand and assist you with the problem, could you please provide more details on the specific issue you are experiencing?
Maryem.
2024-12-20 12:35 AM
Hi,
this is the message I get when I want to connect to my device
(you have the Device ID at the bottom right)
This is the message I got when I want programming
This is on version 2.18
When I replace the XML file from version 2.17 in version 2.18, no more problem
Sébastien
2024-12-20 1:33 AM
Hello @COSEBE ,
Thank you for your feedback.
I tried connecting an STM32H735 (same Device ID 0x483) and downloading a firmware using version 2.18.0 but couldn't reproduce the issues.
Could you please also provide your option bytes configuration? Thank you in advance !
Maryem.
2024-12-20 4:00 AM
You do not use the same device.
Same ID, Yes, but not the same.
Can you check the XML file of ID 483.
Why when I change it, it works. My customer has exactly same problem
Sébastien
2024-12-20 4:11 AM
Value Series part, less/minimal FLASH tested/encoded in part..
Please try exact part as OP
2024-12-20 5:10 AM
I apologize for the oversight. I focused on the Device ID primarily, as I did not have the exact part number on hand at the moment. I will try to obtain it and test with it. I'll update you shortly.
Maryem.
2024-12-26 4:34 PM
Any update on this problem ?
Did you analyse XML file ?
Sébastien
2025-01-02 4:10 AM
Can someone from ST team check the XML file and find a safe workaround ?
Regards,
Sebastien
2025-01-03 5:10 AM
Hello,
I've submitted an internal ticket for our dev team to address this issue,
Internal ticket number: 199559 (This is an internal tracking number and is not accessible or usable by customers)
I will keep you updated about any progress.
Maryem.