cancel
Showing results for 
Search instead for 
Did you mean: 

STM32CubeProgrammer 2.14.0 firmware update error over USB in Windows 10 64 bit

Remo
Associate II

Hi,

similarly to what happened to others with previous versions of STM32CubeProgrammer, an error occurs when I proceed to download the firmware via USB connection:

Error: Write failed at address: 0x800…. (address is not always the same)
Error: failed to download Segment[0]
Error: failed to download the File

The error in log file is:

libusb control transfer error [-9] : LIBUSB_ERROR_PIPE

Even the initial connection via USB does not work correctly, as not all information is always read correctly (The initial connection fails if I use version 2.10.0 of STM32CubeProgrammer).

Similarly to what others have found, everything works correctly if the connection is made through a USB 3.0 hub. Also, everything works fine if I use DfuSeDemo software, so the problem seems to be related to the STM32 BOOTLOADER driver used by STM32CubeProgrammer.

The specs of my system are

microcontroller STM32F072RBT6

firmware version: 0x011a

device id: 0x0448

operating system: Windows 10 Pro 64 bit version 22H2

USB 3.0

Does anyone have any helpful suggestions?

Thanks!

 

 

 

 

6 REPLIES 6
JBurg.5
Associate II

Hi,

I cannot offer a solution but I confirm that there is an issue with the bootloader/STM32 Cube Programmer.

My post regarding the same subject was: https://community.st.com/t5/stm32cubeprogrammer-mcus/stm32cubeprogrammer-dfu-instable/m-p/599084#M5397

I noticed a PC dependent behavior. Using the same boards, on some machines the error always occurs, on others never. As the author of this thread mentioned, it always works with DfuSeDemo.

Regards

Jan

 

The ST USB implementation is not particularly tolerant of USB Hubs or Docking Stations, perhaps how the firmware and drivers react to errors, retries or delays in the communication path. 

Always found direct connectivity work best on Win7 boxes.

Tips, Buy me a coffee, or three.. PayPal Venmo
Up vote any posts that you find helpful, it shows what's working..

Thanks for your reply,

actually, this problem initially occurred in Windows 7, after which it was confirmed by moving to Windows 10

Regards

Thanks for your reply and your post,

regards.

Remo
Associate II
I installed the new version 2.15.0 of STM32CubeProgrammer but the error persists. I also noticed that everything works if I use a USB 3.1 gen 2 port with a Type-C connector and a Type-A to Type-C adapter cable.
 
Veronica1986
Associate

I have the same problem with DFU mode.

I use Cube Programmer version 2.17.0 and uC STM32F765.

Adding a USB hub or a docking station between uC and the PC, the download is always properly done.

I don't know the reason, but I suppose because they introduce delay in the communication.... :face_with_rolling_eyes:

I hope I was helpful to temporarily solving your problem.