2018-10-10 9:42 AM
When running the program STM32CubeProgrammer, an error message appears, saying:
"CubeProgrammer_API or one of its dependencies is missing. Please try reinstalling the program of check your java architecture". However I have the lastest JAVA SE Run Time installed.
Any idea?
OS:
Windows 10 64-bit
Java:
java version "10.0.1" 2018-04-17
Java(TM) SE Runtime Environment 18.3 (build 10.0.1+10)
Java HotSpot(TM) 64-Bit Server VM 18.3 (build 10.0.1+10, mixed mode)
STM32CubeProgrammer version:
[EDITED]1.2.0
Solved! Go to Solution.
2022-04-18 11:15 PM
2022-04-19 1:07 AM
Hello @LLars.1 ,
This is a very old thread and as said @Community member please create a new post on which you describe your problem.
Thanks
Imen