2024-07-09 4:30 AM
Hi,
When installing STM32CubeProgrammer on a Linux machine with a graphical interface, an installation window appears. Now, I want to install STM32CubeProgrammer on a Linux machine without a graphical interface. When I run the installer, I get this error message:
Command line arguments:
SEVERE: com.izforge.izpack.api.exception.IzPackException: Console implementation not found for panel: com.st.CustomPanels.AnalyticsPanels
How can I install STM32CubeProgrammer without the need for a graphical interface?
Best regards,
Solved! Go to Solution.
2024-11-28 5:17 AM
Hello @mikel-m,
The feature is now supported in v2.18.0. It is now possible to install STM32CubeProgrammer via CLI (without using the GUI installer).
You can download it from this Link.
Maryem.
2024-07-09 7:12 AM
Hello @mikel-m,
It is currently not possible to install CubeProgrammer without using the GUI installer or in silent mode. A request has already been submitted to our development team to support this feature. I will keep you updated on any progress.
Internal ticket number: 186141 (This is an internal tracking number and is not accessible or usable by customers).
Maryem.
2024-11-28 5:17 AM
Hello @mikel-m,
The feature is now supported in v2.18.0. It is now possible to install STM32CubeProgrammer via CLI (without using the GUI installer).
You can download it from this Link.
Maryem.