2024-11-01 1:58 AM - edited 2024-11-01 1:59 AM
In the CubeProg, (for instance) the RCC_D1CCIPR value names (*SRC) are different than in the RM 0433 (*SEL). Such things are a bit annoying, if one tries to find things by a keyword search, of if unsure about "is it really the same entity"? Can someone here pass this to the authors for fixing? Thank You!
- CubeProgrammer v2.17.0
- RM0433 Rev. 8, p. 496
Solved! Go to Solution.
2024-11-01 2:14 AM - edited 2024-11-01 2:23 AM
Hello @pkoevesdi
Thank you for feedback that has been escalated for correction on one of the future releases of the STM32CubeProgrammer (under internal ticket number 195558 ).
Best Regards.
STTwo-32
To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
2024-11-01 2:14 AM - edited 2024-11-01 2:23 AM
Hello @pkoevesdi
Thank you for feedback that has been escalated for correction on one of the future releases of the STM32CubeProgrammer (under internal ticket number 195558 ).
Best Regards.
STTwo-32
To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
2024-11-01 2:22 AM
Does this also apply to the names used in the generated source code?
2024-11-01 11:33 PM - edited 2024-11-01 11:33 PM
You mean in CubeMX? Didn't try that, because I don't develop in C. I only use CubeProg for reading and saving registers.
2024-11-02 2:31 AM
@pkoevesdi wrote:You mean in CubeMX?
Yes - the code generated by CubeMX.