2022-01-11 7:39 AM
This is the log:
16:37:14 : STM32CubeProgrammer API v2.8.0
16:37:32 : ST-LINK SN : 003500125553500D20393256
16:37:32 : ST-LINK FW : V3J8M3
16:37:32 : Board : STLINK-V3MINI
16:37:32 : Voltage : 3.00V
16:37:32 : SWD freq : 24000 KHz
16:37:32 : Connect mode: Normal
16:37:32 : Reset mode : Software reset
16:37:32 : Device ID : 0x413
16:37:32 : Revision ID : Rev 2.0
16:37:32 : UPLOADING OPTION BYTES DATA ...
16:37:32 : Bank : 0x00
16:37:32 : Address : 0x40023c14
16:37:32 : Size : 4 Bytes
16:37:32 : UPLOADING ...
16:37:32 : Size : 1024 Bytes
16:37:32 : Address : 0x8000000
16:37:32 : Read progress:
16:37:32 : Data read successfully
16:37:32 : Time elapsed during the read operation is: 00:00:00.002
16:37:36 : Starting Automatic Mode...
16:37:36 : Waiting for device n:1...
16:37:37 : MASS ERASE ...
16:37:45 : Mass erase successfully achieved
16:37:45 : Memory Programming ...
16:37:45 : Opening and parsing file: STM32F401RE-Nucleo_PollingTagDetect.bin
16:37:45 : File : STM32F401RE-Nucleo_PollingTagDetect.bin
16:37:45 : Size : 43524 Bytes
16:37:45 : Address : 0x08000000
16:37:45 : Erasing memory corresponding to segment 0:
16:37:45 : Erasing internal memory sectors [0 2]
16:37:45 : Download in Progress:
16:37:46 : File download complete
16:37:46 : Time elapsed during download operation: 00:00:01.040
16:37:46 : Verifying ...
16:37:46 : Read progress:
16:37:46 : Download verified successfully
16:37:46 : Please disconnect device n:1 and connect the next...
16:37:49 : Waiting for device n:2...
2022-06-10 2:17 AM
Hello @FCiuc.1,
Thank you for posting and sorry for the late reply,
I assume you are using the same STLINK to program different targets.
This feature is implemented in the latest version of STM32CubeProgrammer (v2.10.0) available under this link.
Best regards,
Aziz