2020-11-26 09:50 PM
I want to program the FW via UART.
Read and erase function are working fine, but write function is not working with below error message.
Anybody has a knowhow about this problem?
14:35:12 : Port configuration: parity = even, baudrate = 115200, data-bit = 8, stop-bit = 1.0, flow-control = off
14:35:12 : Activating device: OK
14:35:12 : Chip ID: 0x460
14:35:12 : BootLoader protocol version: 3.1
14:35:14 : UPLOADING OPTION BYTES DATA ...
14:35:14 : Bank : 0x00
14:35:14 : Address : 0x1fff7800
14:35:14 : Size : 52 Bytes
14:35:14 : Bank : 0x01
14:35:14 : Address : 0x1fff7870
14:35:14 : Size : 4 Bytes
14:35:15 : UPLOADING ...
14:35:15 : Size : 131072 Bytes
14:35:15 : Address : 0x8000000
14:35:15 : Read progress:
14:35:30 : Data read successfully
14:35:30 : Time elapsed during the read operation is: 00:00:15.095
14:35:42 : Memory Programming ...
14:35:42 : Opening and parsing file: **
14:35:42 : File : **
14:35:42 : Size : 126 KBytes
14:35:42 : Address : 0x08000000
14:35:42 : Erasing memory corresponding to segment 0:
14:35:42 : Erasing internal memory sectors [0 62]
14:35:43 : Download in Progress:
14:36:13 : Timeout error occured while waiting for acknowledgement.
14:36:13 : Error: Write Operation fails at address 0x8000000
14:36:13 : Error: failed to download Segment[0]
14:36:13 : Error: failed to download the File
14:36:13 : RUNNING Program ...
14:36:13 : Address: : 0x08000000
14:36:43 : Timeout error occured while waiting for acknowledgement.
14:36:43 : Error: START command not acknowledged!
14:36:43 : Error: Start operation failed
14:36:45 : Timeout error occured while waiting for acknowledgement.
14:36:45 : Error: GETID command not acknowledged!
Solved! Go to Solution.
2020-12-02 05:20 PM
For people in the same situation as me, I leave the way I solved.
I tried using the UART built in STLINK-V3, but the above phenomenon occurred.
After that, I tried again using the TTL cable, and it was written correctly.
2020-12-02 05:20 PM
For people in the same situation as me, I leave the way I solved.
I tried using the UART built in STLINK-V3, but the above phenomenon occurred.
After that, I tried again using the TTL cable, and it was written correctly.