2021-11-06 6:25 AM
Erasing memory corresponding to segment 0:
Erasing internal memory sectors [0 64]
Download in Progress:
Error: failed to down
In this case, I am erasing with STM32CubeProgrammer(v2.8.0). When I run it again with STM32CubeIde I get the following message and it works without errors.
Erasing memory corresponding to segment 0:
Erasing internal memory sectors [0 64]
Download in Progress: File download complete
After the application exceeds 128Kb, STM32CubeIde cannot erase the chip. But the application can be written to a previously erased chip.
Thank you
2021-11-07 11:44 PM
I reinstalled STMcubeIde v1.7.0, but when I try to install applications larger than 128kb, I still get the following errors.
Erasing memory corresponding to segment 0:
Erasing internal memory sectors [0 64]
Download in Progress:
Error: failed to download Segment[0]
Error: failed to download the File
Debugger connection lost.
Shutting down...
2021-11-07 11:55 PM
I moved the following files from STMCubeprogrammer to STMCubeIde, but the problem persists.
from E:\Program Files\STMicroelectronics\STM32Cube\STM32CubeProgrammer\bin\FlashLoader\0x467.stldr
to E:\ST\STM32CubeIDE_1.7.0\STM32CubeIDE\plugins\com.st.stm32cube.ide.mcu.externaltools.cubeprogrammer.win32_2.0.0.202105311346\tools\bin\FlashLoader
from E:\Program Files\STMicroelectronics\STM32Cube\STM32CubeProgrammer\Data_Base\STM32_Prog_DB_0x467.xml
to E:\ST\STM32CubeIDE_1.7.0\STM32CubeIDE\plugins\com.st.stm32cube.ide.mcu.externaltools.cubeprogrammer.win32_2.0.0.202105311346\tools\Data_Base
2021-11-08 2:36 AM
STM32CubeIde cannot load applications larger than 128Kb on STM32G0B1VC mcu. I need help with solving this problem.
2022-02-01 7:28 AM
I think, this problem because FlashLoader for 0x467 processor is bad. It can't erase sector 64 and above, because STM32G0B has another page number, Page 64 is 256 for 256k processor (RM0444 page 71).
You can erase all chip STM32_Programmer_CLI.exe -c port=swd -e all
and debug in CubeIDE
2022-02-01 10:35 PM
Thank you for the answer. For full erase operation, "monitor flash mass_erase" for STLink V2 in CubeIDE debug Configuration - Startup - Initialization Commands I added the command. In this way, I can get a full erase before debugging. Similar to STlink-V2, I couldn't find how to do full erase before debug for Segger J-link.
2022-02-01 11:23 PM
In my case, i can't erase all chip. For this, i edit STM32_Prog_DB_0x467.xml and add external tools in CubeIDE.
"C:\Program Files\STMicroelectronics\STM32Cube\STM32CubeProgrammer\bin\STM32_Programmer_CLI.exe" -c port=swd -e [256 271]
And manual erase page, which i need, before start debug