cancel
Showing results for 
Search instead for 
Did you mean: 

Device is under Read Out Protection?

DBalz.1
Associate

Hi all,

i'm tryng to connect to STM32F048T6 by STM32CubeProgrammer.

It is a virgin device, and it starts from System memory and i can see the device like STM32 Bootloader.

When i'm trying to connect using USB in the STM32CubeProgrammer a pop-up message appears reporting: "Deevice is under Read Out Protection, Do you want to disable it?"

I checked the RDP level and is set to AA, so level 0.

Do you have some ideas?

The voltage level are:

VDD = 1.8V

VDDA = 1.8V

VDDIO = 3.3V

I'm using HSI48

This is the CubeProgrammer Log

  10:14:37 : USB speed   : Full Speed (12MBit/s)
  10:14:37 : Manuf. ID   : STMicroelectronics
  10:14:37 : Product ID  : STM32  BOOTLOADER
  10:14:37 : SN          : FFFFFFFEFFFF
  10:14:37 : FW version  : 0x011a
  10:14:37 : Device ID   : unknown
  10:14:37 : Warning: Device is under Read Out Protection
  10:14:37 : Device Read Unprotect requested
  10:14:38 : Disabling memory Read Protection...
  10:14:38 : Memory Read Protection disabled successfully
  10:14:38 : Disconnected from device.

Thanks

Damiano

1 REPLY 1

Hello @Community member​ ,

Please Try using another chip and let me know if you still have the same problem.

Thanks in advance.

BeST Regards,

Walid