2023-07-24 02:10 AM
opens this window:
whereas according to ST's website, current version is newer, 2.14.0:
Can you please comment on this.
Thanks,
JW
Solved! Go to Solution.
2023-07-28 04:33 AM
Hello @waclawek.jan
This is actually a normal behavior that occurs when connection parameters are not set. To solve this issue, please follow the steps below:
After setting the connection parameters, "Software updates" will then detect the latest updates.
Please let me know if you encounter any issues.
Sara.
2023-07-24 08:06 AM
Hi Jan:
I saw similar behavior with STM32CubeProgrammer_CLI (case 00184251 written) with respect to the -help switch response echoing 2.12.0 instead of 2.14.0
regards
Jim Mrowca
2023-07-24 09:16 AM
Has this functionality EVER worked? Been multiple complaints about this for over a year and multiple releases.
2023-07-24 09:43 AM
I don't know. I don't use CubeProgrammer. I just thought today that I may give it a chance again (I tend to give it a chance once a year roughly, but somehow still can't grow to like it).
JW
2023-07-24
03:09 PM
- last edited on
2023-07-25
02:39 AM
by
Lina_DABASINSKA
Has this functionality EVER worked?
Nope, it hasn't. As we know, HAL/Cube development process ir absurdly slow because of "rigorous" testing. Apparently the update functionality, which actually does the update, is such a "rare" scenario that it just didn't occur to the testers.
2023-07-26 06:14 AM
Okay, thanks. Taking note.
JW
2023-07-28 04:33 AM
Hello @waclawek.jan
This is actually a normal behavior that occurs when connection parameters are not set. To solve this issue, please follow the steps below:
After setting the connection parameters, "Software updates" will then detect the latest updates.
Please let me know if you encounter any issues.
Sara.
2023-07-28 05:31 AM - edited 2023-07-28 05:31 AM
Hi @Sara BEN HADJ YAHYA ,
Thanks, that indeed worked.
As two other experienced STM32 users ( @Tesla DeLorean , @Piranha ) both confirmed that updates don't work - and I believe in both cases it was the proxy being set by default - you may perhaps consider a redesign of the download menu to include the proxy setting. It doesn't have any other purpose anyway (unless the integrated spying feature uses it too, but that ought to be removed anyway).
But, to be honest, I recommend a complete redesign of the CubeProgrammer's UI, as it's "modern" (i'd rather call it childish, immature) design with randomly scattered and marked controls, instead of industry standard menus, are very confusing, hard to use, and require unnecessary learning.
And NOBODY needs facebook, twitter, youtube, and [that fourth strange shape] connectivity from a *programming tool*, so just delete those.
JW
2023-07-28 05:44 AM
Well this is broken. I require no proxy and my system proxy settings are set to none.
2023-07-29 02:31 AM - edited 2023-07-29 02:47 AM
As 99% of the users doesn't use any proxy servers, the default "Use System Proxy Parameters" should just work, but it doesn't - therefore it is broken. And the "Check Connection" button seems to do nothing at all, except for changing it's icon.
The fact that the developers didn't even tested whether the update works without a proxy server outside of the ST's internal network, shows how pathetically careless the whole development process is. And it also means that nobody of them are actually using that software at home, which shows the background of those people - they are not genuinely interested in these technologies.