2024-04-02 07:18 AM
"My STM32 is locked out of its program. How can I unlock it? I need to continue learning to use it, even though I've just started."
STMicroelectronics ST-LINK GDB server. Version 7.5.0
Copyright (c) 2023, STMicroelectronics. All rights reserved.
Starting server with the following options:
Persistent Mode : Disabled
Logging Level : 1
Listen Port Number : 31234
Status Refresh Delay : 15s
Verbose Mode : Disabled
SWD Debug : Enabled
InitWhile : Enabled
Target no device found
Error in initializing ST-LINK device.
Reason: No device found on target.
2024-04-25 08:17 AM
Hello @bbb,
Could you please provide further details : Which part number are you using ? Are you using a custom board ? Can you connect in CubeProgrammer standalone version ?
Thanks in advance,
Aziz
2024-04-25 09:14 AM
They make literally hundreds of "STM32", could you narrow this down a tad, and provide some context to your question.
Try jumpering / pulling BOOT0 HIGH, to VDD, will stop your broken code from running.