cancel
Showing results for 
Search instead for 
Did you mean: 

Connection issue

bbb
Associate

"My STM32 is locked out of its program. How can I unlock it? I need to continue learning to use it, even though I've just started."

 

STMicroelectronics ST-LINK GDB server. Version 7.5.0

Copyright (c) 2023, STMicroelectronics. All rights reserved.

 

Starting server with the following options:

Persistent Mode : Disabled

Logging Level : 1

Listen Port Number : 31234

Status Refresh Delay : 15s

Verbose Mode : Disabled

SWD Debug : Enabled

InitWhile : Enabled

 

Target no device found

 

Error in initializing ST-LINK device.

Reason: No device found on target.

 

2 REPLIES 2
Aziz BRIGUI
ST Employee

Hello @bbb,

Could you please provide further details : Which part number are you using ? Are you using a custom board ? Can you connect in CubeProgrammer standalone version ?

Thanks in advance,

Aziz


In order to give better visibility on the answered topics, please click on 'Accept as Solution' on the reply which solved your issue or answered your question.

They make literally hundreds of "STM32", could you narrow this down a tad, and provide some context to your question.

Try jumpering / pulling BOOT0 HIGH, to VDD, will stop your broken code from running.

Tips, Buy me a coffee, or three.. PayPal Venmo
Up vote any posts that you find helpful, it shows what's working..