cancel
Showing results for 
Search instead for 
Did you mean: 

Can't program 128bit data in STM32U5 OTP area with Programmer 2.17.0

DMoim.1
Associate II

Hi,

I've tried to program OTP area of STM32U575 at address 0x0BFA0010 with a quad-word (4x32bit of data) but only half are programmed (the first half) while the 2 remaining words are at 0xFFFFFFFF (erased state) and cannot be programmed anymore.

I've loaded a binary file with 128bits of data, chose the download attress at 0x0BFA0010 and pushed the download button.

Accoding to the datasheet the flash must be programmed 128bit at once: is that implemented in the programmer?

Best regards,

 Diego

3 REPLIES 3
Imen.D
ST Employee

Hello @DMoim.1 

I'm checking internally this issue (tracked via internal ticket: 196262)

We will keep you updated here when progress is made in this request.

Thank you for your contribution.

When your question is answered, please close this topic by clicking "Accept as Solution".
Thanks
Imen
Imen.D
ST Employee

Hi @DMoim.1  

Issue is confirmed and our Dev team are working to resolve it.

In the meantime, you can try using Cubeprogrammer version 2.15.0. 

Thank you for your contribution.

When your question is answered, please close this topic by clicking "Accept as Solution".
Thanks
Imen
Maryem
ST Employee

Hello @DMoim.1 ,

 

The issue has been fixed in STM32CubeProgrammer v2.19.0

You can download it from this Link.

 

Maryem.


In order to give better visibility on the answered topics, please click on 'Accept as Solution' on the reply which solved your issue or answered your question.