cancel
Showing results for 
Search instead for 
Did you mean: 

Installation problems with CubeIDE 1.18.1 on Fedora 42

xuraax
Associate III

Hi

Last week I installed the latest version of stm32CubeIDE on my Fedora 42 system using the generic linux installer from the ST web site.

 

The installation went smoothly and I was able to run the program and even generate a simple project.

When I went back 2 days later to continue, each time i ran CubeIDE the system starts and displays the standard "workspace" window. Upon hitting enter a small empty windows comes up and the system hangs there. The app does not appear to close since if I try to start again I get the message that the app is already running.

Any ideas please?

 

1 ACCEPTED SOLUTION

Accepted Solutions
xuraax
Associate III

Hi @Ghofrane GSOURI ,

 

Thank you for your reply.  Following my initial mail I had discovered that 1.19.0 had come out.

I deleted everything related to 1.18.1. This was not so simple as the use of uninstall.sh file did not clear everything.

I then downloaded the RPM version of the software. Previously I had installed the generic linux version. There was also an update to Fedora which I installed.

I then ran the .sh file using sudo and indeed the installation seems to have been successful. Since initially the 1.18.1 had also ran properly for a few days I will wait a few more days before declaring that the issue is solved.

Thanks for your help.

View solution in original post

2 REPLIES 2
Ghofrane GSOURI
ST Employee

Hello @xuraax 

Reinstalling STM32CubeIDE with the latest version 1.19.0 is recommended if you continue to experience issues such as the IDE hanging after workspace selection. A fresh installation can resolve corrupted files, missing dependencies, or configuration problems that may have occurred during the initial setup, ensuring a clean and stable development environment on your Fedora 42 system.

  LINK for download 

I will be waiting for your feedback.

THX

Ghofrane

 

 

To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.

xuraax
Associate III

Hi @Ghofrane GSOURI ,

 

Thank you for your reply.  Following my initial mail I had discovered that 1.19.0 had come out.

I deleted everything related to 1.18.1. This was not so simple as the use of uninstall.sh file did not clear everything.

I then downloaded the RPM version of the software. Previously I had installed the generic linux version. There was also an update to Fedora which I installed.

I then ran the .sh file using sudo and indeed the installation seems to have been successful. Since initially the 1.18.1 had also ran properly for a few days I will wait a few more days before declaring that the issue is solved.

Thanks for your help.