2022-02-24 12:25 AM
2022-02-24 02:23 AM
This is a screenshot of STM32CubeProgrammer which is connected to STM32H747-DIISCO board.
RDP option is available from OB (Option bytes) menu.
2022-02-24 02:02 AM
You probably mean RDP = Readout Protection?
This function is of course also included in the STM32H7 series - see e.g. in RM0399, section 4.5.3.
Does it answer your question?
Regards
/Peter
2022-02-24 02:23 AM
This is a screenshot of STM32CubeProgrammer which is connected to STM32H747-DIISCO board.
RDP option is available from OB (Option bytes) menu.
2022-02-24 06:52 AM
> I have seen in the document that setting RDB feature works only in stm32f series.
What document?