cancel
Showing results for 
Search instead for 
Did you mean: 

Can I lock stm32h747 chip by setting RDB level in stm32programmer ? I have seen in the document that setting RDB feature works only in stm32f series.

SLuit.1
Associate III
1 ACCEPTED SOLUTION

Accepted Solutions
mƎALLEm
ST Employee

This is a screenshot of STM32CubeProgrammer which is connected to STM32H747-DIISCO board.

RDP option is available from OB (Option bytes) menu.

0693W00000KaNgRQAV.png

To give better visibility on the answered topics, please click on "Accept as Solution" on the reply which solved your issue or answered your question.

View solution in original post

3 REPLIES 3
Peter BENSCH
ST Employee

You probably mean RDP = Readout Protection?

This function is of course also included in the STM32H7 series - see e.g. in RM0399, section 4.5.3.

Does it answer your question?

Regards

/Peter

In order to give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
mƎALLEm
ST Employee

This is a screenshot of STM32CubeProgrammer which is connected to STM32H747-DIISCO board.

RDP option is available from OB (Option bytes) menu.

0693W00000KaNgRQAV.png

To give better visibility on the answered topics, please click on "Accept as Solution" on the reply which solved your issue or answered your question.
TDK
Guru

> I have seen in the document that setting RDB feature works only in stm32f series.

What document?

If you feel a post has answered your question, please click "Accept as Solution".