2024-06-16 07:29 PM
If driver porting is successful, reading and writing eMMC from STM32CubeProgrammer should be feasible.
I have tested that the read, write eMMC functions are ok and implemented in read, write, MassErase and SectorErase functions of Loader , but from the STM32CubeProgrammer it always fails.
Can anyone help me?
MCU: STM32H743BIT6
eMMC: ISSI IS21ES08G-JQLI
2024-06-21 02:21 AM - edited 2024-06-21 02:22 AM
Hello @Louie ,
Could you please share the error message?
Does this error recur when using the latest version of STM32CubeProgrammer?