cancel
Showing results for 
Search instead for 
Did you mean: 

Arm64 with Snapdragon X plus process unable to detect st link

PChat.4
Associate

I bought an arm64 based PC a few months ago and I have been unable to connect to or detect stlink even after installing driver, is there a work around? has anyone successfully been able to use the snapdragon processor with stlink? is there another kind of debugger that works with arm based pc's? your help will be highly appreciated, thanks

2 REPLIES 2

What OS are you running on this PC ?

 


@PChat.4 wrote:

 I have been unable to connect to or detect stlink 


You mean it doesn't even show up in Device Manager (or equivalent) ?

 

Have you seen this:

https://community.st.com/t5/stm32-mcus/faq-possible-communication-failure-between-stlink-v3-and-some/ta-p/736578

 

Also:

https://community.st.com/t5/stm32-mcus/how-to-solve-debugger-connection-issues/tac-p/698105/highlight/true#M956

Ozone
Lead III

OpenOCD is available for Linux, and supports the ST-Link.
I'm pretty sure ARM/ARM64 repositories of most distros provide packages.

As far as Windows for ARM is concerned, you will probably depend on ST to release appropriate drivers.