2024-07-31 08:18 AM
I appreciate that something has been changed in this are - I see sector numbering is being different (strange but at least different)
But in the end of the day DFU upload is still broken
erasing sector 0005 @: 0x08020000 done erasing sector 0006 @: 0x08040000 done erasing sector 0007 @: 0x08060000 done erasing sector 24786 @: 0x08080000 done Download in Progress: ±±±±±±±±±±±±±±±±±±±±±±±±±±±±±±±±±±±±±±±±±±±±±±±±±± 0% 2% 4% 6% 8% 10% 12% 14% 16% 18% 20% 22% 24% 26% 28% 30% 32% 34% 36% 38% 40% 42% 44% 46% 48% 50% 52% 54% 56% 58% 60% 62% 64% 66% 68% 70% 72% 74% 76% 78% 80% 82% 84% 86% 88% 90% 92% 94% 96% 98% 100% File download complete Time elapsed during download operation: 00:00:21.193 Verifying ... Read progress: ±±±±±±±±±±±±±±±±±±±±±±±±±±±±±±±±±±±±±±±±±±±±±±±±±± 50% 2% 4% 6% 8% 10% 12% 14% 16% 18% 20% 22% 24% 26% 28% 30% 32% 34% 36% 38% 40% 42% 44% 46% 48% 50% 52% 54% 56% 58% 60% 62% 64% 66% 68% 70% 72% 74% 76% 78% 80% 82% 84% 86% 88% 90% 92% 94% 96% 98% 100% Error: Data mismatch found at address 0x08080000 (byte = 0x00 instead of 0x49) Error: Download verification failed
if it helps feel free to test using rusefi.bin file from https://rusefi.com/build_server/rusefi_bundle_proteus_f7.zip