2023-03-23 5:53 AM
Hi, when I use the cubemx to config the stm32h743iit6 project, the clock system shows some error as below. But I try it on another PC, and the same config can work well.
I don't know why?
Solved! Go to Solution.
2023-03-23 6:27 AM
Hello @Junde ,
For the STM32H743 , we have 3 revisions : V , Y and X. (errata sheet)
Use silicon revision V devices to reach a maximum frequency of 480 MHz.
Please make sure which revision you have and you can refer to :
Foued
To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
2023-03-23 6:27 AM
Hello @Junde ,
For the STM32H743 , we have 3 revisions : V , Y and X. (errata sheet)
Use silicon revision V devices to reach a maximum frequency of 480 MHz.
Please make sure which revision you have and you can refer to :
Foued
To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
2023-03-23 7:34 AM
@KHALSI_Foued
Thanks for your reply.
As per your description, there are different revisions on RCC config page(but just rev.Y and rev.V, NO rev.X).
And I want to know how to make sure which revision the chip I have is.
Just see the silk print on the chip surface?
2023-03-24 1:23 AM
Yes, you can just look at your MCU.
Or try to connect your board to the STM32CubeProgrammer.
Foued
To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.