cancel
Showing results for 
Search instead for 
Did you mean: 

Why does my program always go into HardFault_Handler?

plpc.1
Associate II

I just make a simple test. My cpu is stm32F303VET6,. Use Stm32cubeMx to generate a simple project with few lines of code, like:

int main(void)

{

 /* USER CODE BEGIN 1 */

 /* USER CODE END 1 */

 /* MCU Configuration--------------------------------------------------------*/

 /* Reset of all peripherals, Initializes the Flash interface and the Systick. */

 HAL_Init();

 /* USER CODE BEGIN Init */

 /* USER CODE END Init */

 /* Configure the system clock */

 SystemClock_Config();

 /* USER CODE BEGIN SysInit */

 /* USER CODE END SysInit */

 /* Initialize all configured peripherals */

 MX_GPIO_Init();

 /* USER CODE BEGIN 2 */

 /* USER CODE END 2 */

 /* Infinite loop */

 /* USER CODE BEGIN WHILE */

 while (1)

 {

  /* USER CODE END WHILE */

  /* USER CODE BEGIN 3 */

 }

 /* USER CODE END 3 */

}

But everytime when it runned to MX_GPIO_Init(), then it was dead. And i found it hanged in HardFault_Handler(void). why?

4 REPLIES 4

Look at the instructions and registers at the point it faulted.

Tips, Buy me a coffee, or three.. PayPal Venmo
Up vote any posts that you find helpful, it shows what's working..
Karl Yamashita
Principal

Upload your ioc file

Don't worry, I won't byte.
TimerCallback tutorial! | UART and DMA Idle tutorial!

If you find my solution useful, please click the Accept as Solution so others see the solution.

ok, please check the attached file. Thanks

sorry, i uploaded a wrong ioc file. this is the correct one.​