2018-11-23 4:26 AM
2018-11-30 7:14 AM
When "Generate Under Root" checkbox is set the code generator doesn't create the TrueSTUDIO folder.
When "Generate Under Root" checkbox is not set it creates a TrueSTUDIO folder and places the project files, the startup file and syscalls.c there.
2018-11-23 5:45 AM
Hello,
Could you please describe the scenario that you followed in this case and which STM32CubeMX version is used, so that it will be easier to reproduce it.
Kind Regards,
Imen
2018-11-23 7:19 AM
I don't remember the scenario - I was busy with something else for a week or so.
CubeMX was 4.27.0 and Atollic was 9.1.0 (and they still are the used versions).
The TrueSTUDIO folder contains "startup_stm32f427xx.s" and folder "cubemx".
The cubemx folder contains folder ".settings" and files ".cproject", ".project", "cubemx.elf.launch" and "STM32F427ZG_FLASH.ld".
Sounds like some kind of backup, but could be something else too.
2018-11-23 8:07 AM
Hello,
I cannot reproduce your case using STM32CubeMx version 5.0.0
Can you please check if this issue is reproduced with the last STM32CubeMx version 5.0.0
Kind Regards,
Imen
2018-11-25 12:04 PM
I'm sorry, but I don't think so. I don't have the time.
It happened at work.
On the other hand, there seems to be no harm of it.
I try to check if it's just a backup when a new (fixed) project was generated on top of the old.
2018-11-26 2:54 AM
Yes, they look like backup - telling by the file dates.
2018-11-30 7:01 AM
Hello @turboscrew
I can not answer your question until I have more details.
Please send me your ioc file so you can tell the difference between 4.27 and 5.0.
Best regards,
Wael
2018-11-30 7:14 AM
When "Generate Under Root" checkbox is set the code generator doesn't create the TrueSTUDIO folder.
When "Generate Under Root" checkbox is not set it creates a TrueSTUDIO folder and places the project files, the startup file and syscalls.c there.
2018-11-30 8:00 AM
Hello @After Forever @turboscrew
I tried with cuibeMX 5.0.0 and it works to perfection as you want
try on your part and once you find a problem contact me.
I will always be at your service and your availability at any time
Best regards
Wael
2018-11-30 10:50 AM
Thanks!!