2023-11-30 10:34 AM
Hi
When selecting azure RTOS in CubeMX, it is not possible to select FATFS. FATFS is greyed out. It is only allowed to choose FileX. Why?
Thx
2023-11-30 10:53 AM - edited 2023-11-30 10:54 AM
Because it's Microsoft, properly integrated and licensed.
ST hasn't updated FATFS in something like 6 or 7 years, it has some nasty bugs, and clearly no one is interested in integration and testing tasks. Heck that would require regression testing over a dozen STM32 families.
Stop relying on code generators to create code and make choices. If you want different outcomes, make different choices..
2023-12-05 03:51 AM
Hello @MK..1 ,
To check the issue, could you please precise:
Which STM32 devices are you using?
Which STM32CubeMx version are you using?
Thank you.
Kaouthar
To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
2023-12-05 07:16 AM
I am using STM32F446ZCJx and STM32CubeIDE Version: 1.14.0 and
STM32Cube FW_F4 V1.27.1
2023-12-06 03:05 AM
Hi @MK..1 ,
I reported this issue internally.
Internal ticket number: 168051 (This is an internal tracking number and is not accessible or usable by customers).
Thank you for your contribution in STCommunity
Kaouthar
To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.