USB STM32G0B1KCT6 not working
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
2023-01-12 8:00 AM
Hi
I have used STMCubeIDE 1.11.0 (Cube 1.6.1) to generate the code for USB CDC interface for STM32G0B1.
The code is as CubeMX would generate. I have not modified the code at all.
When I plug the device into a PC I get "USB device not recognized" I have increased the heap and stack to be 0x1000. without any luck.
What can I try to try to figure out what the issue is.
Thanks,
Solved! Go to Solution.
- Labels:
-
STM32CubeIDE
-
STM32CubeMX
-
STM32G0 Series
-
USB
Accepted Solutions
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
2023-01-16 3:37 AM
Hi.
It is now working. I used a STM32G474 example code to figure out what is wrong.
There was 3 errors in the auto generate code.
The 48MHz clock was not started.
Missing USBD_Clock_Config();
in void MX_USB_Device_Init(void))
The USB interrupt was not enabled
Missing
HAL_NVIC_SetPriority(USB_UCPD1_2_IRQn , 6, 0);
HAL_NVIC_EnableIRQ(USB_UCPD1_2_IRQn);
in void HAL_PCD_MspInit(PCD_HandleTypeDef* pcdHandle))
The USB interrupt Handler was not present.
void USB_UCPD1_2_IRQHandler(void)
{
HAL_PCD_IRQHandler(&hpcd_USB_DRD_FS);
}
Thanks
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
2023-01-12 11:40 PM
Hello @DCorn
First let me thank you for posting.
For the USB CDC, it is important to configure the USB clock to the correct frequency, typically 48 MHz This clock is derived from the system clock, so it is also important to ensure that the system clock is configured to the correct frequency as well.
Thx
Ghofrane
To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
2023-01-13 1:32 AM
Hi
As you can see the internal 48MHz clock is by default linked to the USB. So that's not the issue I think. I have even tried setting Pclk to be 48MHz still did not work.
David
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
2023-01-13 1:39 AM
Hello again @DCorn
Let's try this :
-Make sure that the USB cable you are using is functioning properly.
-Make sure that all the necessary drivers are installed on the PC, and that the device is listed in the device manager.
-You can also try using different USB port or computer to check if the problem is with your PC or the device.
Thx
Ghofrane
To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
2023-01-16 3:37 AM
Hi.
It is now working. I used a STM32G474 example code to figure out what is wrong.
There was 3 errors in the auto generate code.
The 48MHz clock was not started.
Missing USBD_Clock_Config();
in void MX_USB_Device_Init(void))
The USB interrupt was not enabled
Missing
HAL_NVIC_SetPriority(USB_UCPD1_2_IRQn , 6, 0);
HAL_NVIC_EnableIRQ(USB_UCPD1_2_IRQn);
in void HAL_PCD_MspInit(PCD_HandleTypeDef* pcdHandle))
The USB interrupt Handler was not present.
void USB_UCPD1_2_IRQHandler(void)
{
HAL_PCD_IRQHandler(&hpcd_USB_DRD_FS);
}
Thanks
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
2023-01-16 4:19 AM
Hello @DCorn
Let's do those steps :
1-Create project in CubeMX
2-USB-->Device FS
3-RCC-->Select HSE clock-->(Bypass clock source )
4- Select CDC class in MiddleWares
5-Go to clock configuration --> Set 8 MHz as input frequency
6-Make sure that the frequency for USB CDC is 48Mhz
Please try this solution and I will be waiting for your feedback don't hesitate to raise any question
Thx
Ghofrane
To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
2023-08-31 7:52 AM
Thanks @DCorn!
I also added the missing clock configuration and increased heap size to 0x1000. The IRQ is now as you mentioned (FW_G0_V1.6.1). But I still get the message "USB device not recognized".
Interestingly, I can measure a 1.5 k pull-up on D- pin instead of D+ pin like it's a low speed device (the pin-out is correct).
Have you got suggestions what else to check?
Thank you!
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
2023-12-21 10:49 AM
Hi,
Struggling with the same problem here. I think @DCorn solution was pointed in the right direction but didn't work for me because some of the functions to add just doesn't exist in my environment.
I fixed it in the graphical Pinout & Configuration tool:
go to 'System Core' -> 'NVIC' and enable 'USB, UCPD1 and UCPD2 global interrupts'. Save the configuration to regenerate the code and try again.
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
2025-05-20 12:06 PM
Hi, I have the same issue. I checked my code and all the following lines are generated from CubeMX
HAL_NVIC_SetPriority(USB_UCPD1_2_IRQn , 6, 0);
HAL_NVIC_EnableIRQ(USB_UCPD1_2_IRQn);
void USB_UCPD1_2_IRQHandler(void)
{
HAL_PCD_IRQHandler(&hpcd_USB_DRD_FS);
}
But I can't find anything about USBD_Clock_Config();
Can you explain this function please?
Thank you