2022-08-09 05:47 AM
Hello
I'm using a stm32L431. here the documentation :
https://www.st.com/en/microcontrollers-microprocessors/stm32l4x1.html#documentation
HSI is enabled at 16MHz for USART2, used to receive a 1200Bd signal (7bit data + even parity + 1 stop).
I receive wrong characters because of the trim. of parity
I already asked a question about the TRIM but that's not the problem
https://community.st.com/s/question/0D53W00001iwHrbSAE/how-to-trim-the-stm32-hsi-easily
I connect a USB converter (With FT232) on the RX of UART2 to send data to the stm32
I use CubeMx to configure UART2
>> Case 1 that works : (no parity)
Configuration by CubeMX :
huart2.Instance = USART2;
huart2.Init.BaudRate = 1200;
huart2.Init.WordLength = UART_WORDLENGTH_8B;
huart2.Init.StopBits = UART_STOPBITS_1;
huart2.Init.Parity = UART_PARITY_NONE;
huart2.Init.Mode = UART_MODE_RX;
huart2.Init.HwFlowCtl = UART_HWCONTROL_NONE;
huart2.Init.OverSampling = UART_OVERSAMPLING_16;
huart2.Init.OneBitSampling = UART_ONE_BIT_SAMPLE_DISABLE;
huart2.AdvancedInit.AdvFeatureInit = UART_ADVFEATURE_NO_INIT;
if (HAL_UART_Init(&huart2) != HAL_OK)
Teraterm configuration :
I receive the data without fault...
>> Case 2 not working : (even parity)
Configuration by CubeMX :
huart2.Instance = USART2;
huart2.Init.BaudRate = 1200;
huart2.Init.WordLength = UART_WORDLENGTH_8B; // including parity
huart2.Init.StopBits = UART_STOPBITS_1;
huart2.Init.Parity = UART_PARITY_EVEN;
huart2.Init.Mode = UART_MODE_RX;
huart2.Init.HwFlowCtl = UART_HWCONTROL_NONE;
huart2.Init.OverSampling = UART_OVERSAMPLING_16;
huart2.Init.OneBitSampling = UART_ONE_BIT_SAMPLE_DISABLE;
huart2.AdvancedInit.AdvFeatureInit = UART_ADVFEATURE_NO_INIT;
if (HAL_UART_Init(&huart2) != HAL_OK)
Teraterm configuration :
Here I receive wrong things, part of the characters are correct, another incoherent
I know that the probability is high that the problem is between the keyboard and the chair but... I'm standing, without a chair! so it can come from a concern of HAL as for the TRIM which is strangely managed?
Thanks in advance
Solved! Go to Solution.
2022-08-09 06:08 AM
You will need to mask the parity bit off data read in such a fashion
ie int data = USART2->RDR & 0x7F; // mask down to 7-bit
2022-08-09 06:02 AM
> Teraterm configuration :
Probably failed screenshot insertion? Try through uploading, on bottom of the editor window click on the "picture" icon.
Also, read out the USART registers content and check/post.
JW
2022-08-09 06:08 AM
You will need to mask the parity bit off data read in such a fashion
ie int data = USART2->RDR & 0x7F; // mask down to 7-bit
2022-08-09 06:26 AM
>> Case 1 that works : (no parity)
>> Case 2 not working : (even parity)
2022-08-09 06:34 AM
I'm afraid to understand...
When using parity do we need to manually remove the parity bit?
Here I recover the data by the DMA ; I have to loop on all my buffer to delete the 7th bit of all buffer éléments ?
I'm testing...it would correspond well to the fact that some characters pass and others do not
2022-08-09 06:54 AM
it's all good with less 7 bit, Thanks a lot
I think I've never had to fetch data on 7b before, maybe every uart in the world works like this; I wouldn't have suspected it for a second
2022-08-09 07:13 AM
Probably no other UART in the world works like this...
Glad you got it working. Clive (Tesla) is the local expert of all things weird... 🙂
JW
2022-08-09 07:27 AM
I shave with Occam's Razor...
I suppose they saved a bunch of transistors with this design. The holding registers are 9-bit wide, the DR reads/writes as a 16-bit value. I'd assume the TDR has logic in-front of it to selectively compute the parity bit, and the RDR has logic behind to selectively check, and you're left to mask the value you read. Makes for a simpler, orthogonal, design.
Makes sense to the IC/HW guys, less so the SW ones
2022-08-09 07:28 AM
thank you
big stress on the starting point of my test
but I'm reassured, all my other tests (error, frame, frame analysis...) work perfectly.