Unable to Read and Write to I2C EEPROM
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2017-02-23 12:43 PM
I am using atmega AT24C256 EEPROM and STM32F0 discovery module. I am struggling to read/Write to the memory. Here is the example I trying to use:-
&sharpdefine I2C1_DEVICE_ADDRESS 0x50 /* A0 = A1 = A2 = 0 */
&sharpdefine MEMORY_ADDRESS 0x07Buffer[0] = 'M';
HAL_I2C_Mem_Write(&hi2c1, (uint16_t) I2C1_DEVICE_ADDRESS<<1, MEMORY_ADDRESS, 1, Buffer, 1, 5); HAL_Delay(1000); Buffer[0] = 0x00; HAL_Delay(1000); HAL_I2C_Mem_Read(&hi2c1, (uint16_t) I2C1_DEVICE_ADDRESS<<1, MEMORY_ADDRESS, 1, Buffer, 1, 5); if (Buffer[0] == 0x4D) // if xBuffer[0] = 'M' { Test = 1; }On reading from memory, I do not get the 'M' or but some '255' instead. Where is the problem? Do I need to configure clock properly? I used CUBEMX for basic routines.
#cubemx #eeprom #hal #stm32f0 #i2c- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2017-02-23 4:32 PM
this works for me, maybe it helps you. 'addr' is the register address in the eeprom you want to read.
uint8_t read_eeprom_reg(uint16_t addr)
{ uint8_t buffer[] = {addr}; uint8_t value; while (HAL_I2C_GetState(&hi2c1) != HAL_I2C_STATE_READY) {}
while (HAL_I2C_IsDeviceReady(&hi2c1, (uint16_t)(0x50<<1), 3, 100) != HAL_OK) { }
while (HAL_I2C_Master_Transmit(&hi2c1, // i2c handle (uint16_t)(0x50<<1), // i2c address, left aligned (uint8_t *)&buffer, // data to send 2, // how many bytes - 16 bit register address = 2 bytes 100) // timeout != HAL_OK) // result code { if (HAL_I2C_GetError(&hi2c1) != HAL_I2C_ERROR_AF) {Error_Handler();
} }while (HAL_I2C_IsDeviceReady(&hi2c1, (uint16_t)(0x50<<1), 3, 100) != HAL_OK) {}
while (HAL_I2C_Master_Receive(&hi2c1, // i2c handle (uint16_t)(0x50<<1), // i2c address, left aligned (uint8_t *)&value, // pointer to address of where to store received data 1, // expecting one byte to be returned 100) // timeout != HAL_OK) // result code { if (HAL_I2C_GetError (&hi2c1) != HAL_I2C_ERROR_AF) {Error_Handler();
} }return value;
}
void write_eeprom_reg(uint16_t reg_addr, uint8_t value)
{ uint8_t d[3];d[0] = (reg_addr >> 8) & 0xFF; // high byte of 16-bit register address
d[1] = (reg_addr) & 0xFF; // low byte of 16-bit register address d[2] = value; // what value are we writing to the registerwhile (HAL_I2C_IsDeviceReady(&hi2c1, (uint16_t)(0x50<<1), 3, 100) != HAL_OK) {}
if (HAL_I2C_Master_Transmit(&hi2c1, // i2c handle (uint16_t)(0x50<<1), // i2c address, left aligned (uint8_t *)d, // pointer to the buffer containing the data sizeof(d), // how many bytes are we transmitting 1000) // timeout value != HAL_OK) // result code {Error_Handler();
} else { //printf('Master transmit successful\r\n'); }}
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2017-02-25 3:05 AM
Euh... 256kbit = 32kbyte a single byte for the memory address location might be too short...
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2017-02-28 9:29 PM
do you have an example of that function looping the eeprom?
for me has been very hard trying to control an AT24C32 with 0x57 address,.
uint8_t eeprominfo;
write_eeprom_reg(0x00,0x4D);
HAL_Delay(500);
eeprominfo = read_eeprom_reg(0x00);
was trying this with not luck, thanks.
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2017-03-01 1:06 AM
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2017-03-01 9:38 AM
thanks for the example i have tried to use that but it does not work with hal projects,
i chose not to work with stdperiph and learn Hall Drivers since its the ST path
but it has been really hard since i have not been able to write to AT24C32 or AT24C0, i have used everything i have found in the web, i know the chip its ok since i have an arduino to test the components and check the address.
would be awesome to see an example using johndoe classes
uint8_t eeprominfo;
write_eeprom_reg(0x00,0x4D);
HAL_Delay(500);
eeprominfo = read_eeprom_reg(0x00);
i also tried this.
♯ define I2C1_DEVICE_ADDRESS 0x57
♯ define MEMORY_ADDRESS 0x07Buffer[0] = 'M';
HAL_I2C_Mem_Write(&hi2c1, (uint16_t) I2C1_DEVICE_ADDRESS<<1, MEMORY_ADDRESS, 1, Buffer, 1, 5); HAL_Delay(1000);Buffer[0] = 0x00;HAL_Delay(1000);HAL_I2C_Mem_Read(&hi2c1, (uint16_t) I2C1_DEVICE_ADDRESS<<1, MEMORY_ADDRESS, 1, Buffer, 1, 5); if (Buffer[0] == 0x4D) // if xBuffer[0] = 'M'{Test = 1;}also not results i tried many things like the first poster on this thread,
please help if u know what im doing wrong, thanks.
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2017-03-01 10:34 AM
Ok, back to original code:
Try this:
Buffer[0] = 'M';
HAL_I2C_Mem_Write(&hi2c1, 0xA0, 0x0007, 2, Buffer, 1, 5);
HAL_Delay(10);
Buffer[0] = 0x00;
HAL_I2C_Mem_Write(&hi2c1, 0xA0,
0x0007
, 2, Buffer, 0, 5);
HAL_I2C_Mem_Read(&hi2c1, 0xA1, 0x0007, 2, Buffer, 1, 5);
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2017-03-01 7:50 PM
thank you, for ur answer but it does not work too
:(
i changed the address to 0x57 since is the address of the AT24C32 in the circuit, (arduino reads it ok)
tried changing the values for example to 0x00, 0x01, 0x02, 0x03 of the reg address and checking back the value but nothing,
i can read from other i2c devices but not the eeprom.
Buffer[0] = 'M';
HAL_I2C_Mem_Write(&hi2c1, 0x57, 0x0007, 2, Buffer, 1, 5);
HAL_Delay(10);
Buffer[0] = 0x00;
HAL_I2C_Mem_Write(&hi2c1,
0x57
,0x0007
, 2, Buffer, 0, 5);
HAL_I2C_Mem_Read(&hi2c1,
0x57
, 0x0007, 2, Buffer, 1, 5);- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2017-03-02 2:20 AM
Your eeprom is probably not powered, or SDA/SCL crossed or WP pin level is wrong, or bad soldering. Should be typically something obviously simple that is missed. Take a step back and contemplate the board.
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2017-03-02 8:21 PM
its not my friend , when switched to the arduino it reads it ok.
its the DS3231 AT24C32 IIC Module (this one
http://www.icstation.com/images/big/productimages/2416/2416.JPG
)can read the DS3231 rtc at the 0xD0 address with :
I2C_ReadBuffer(hi2c1,(uint16_t)0xD0,7); // function writes to
aTxBuffer
year = aTxBuffer[6]; year = RTC_ConvertFromDec(year); month = aTxBuffer[5]; month = RTC_ConvertFromDec(month); date = aTxBuffer[4]; date = RTC_ConvertFromDec(date); day = aTxBuffer[3]; day = RTC_ConvertFromDec(day);but cant get or write any data to the ATC32 at the 0x57 with the Hall Library.