2020-02-26 8:14 AM
I want to use only the Tx pin on UART4, it is on PA0/CN5-1 of the Arduino connector. I setup
// Initialize UART4 for Debug Terminal 250 kbaud using 50 MHz PCLK1 /////////////////////////////////
PeriphClkInitStruct.PeriphClockSelection = RCC_PERIPHCLK_TIM
|RCC_PERIPHCLK_USART1
|RCC_PERIPHCLK_USART6
|RCC_PERIPHCLK_UART4; // enable clocks to USART1/USART6/UART4/TIM
PeriphClkInitStruct.Usart1ClockSelection = RCC_USART1CLKSOURCE_PCLK2; // USART1 runs on PCLK2 = 100 MHz
PeriphClkInitStruct.Usart6ClockSelection = RCC_USART6CLKSOURCE_PCLK2; // USART6 runs on PCLK2 = 100 MHz
PeriphClkInitStruct.Usart6ClockSelection = RCC_UART4CLKSOURCE_PCLK1; // USART4 runs on PCLK1 = 50 MHz
PeriphClkInitStruct.TIMPresSelection = RCC_TIMPRES_ACTIVATED;
RCC->APB1ENR |= RCC_APB1ENR_UART4EN;
__HAL_RCC_GPIOA_CLK_ENABLE();
GPIO_InitStruct.Alternate = GPIO_AF8_UART4;
GPIO_InitStruct.Mode = GPIO_MODE_OUTPUT_PP; // PA0=Tx
GPIO_InitStruct.Pin = GPIO_PIN_0;
GPIO_InitStruct.Pull = GPIO_NOPULL;
GPIO_InitStruct.Speed = GPIO_SPEED_MEDIUM;
HAL_GPIO_Init(GPIOA, &GPIO_InitStruct);
UART4->CR1 = 0x00; // reset
UART4->BRR = 400; // 100,000,000/2/250000=200 (running on PCLK1 = 50 MHz)
UART4->CR1 = 0x1008; // Enable Tx and 9-bit length using bit12=1
UART4->CR1 |= USART_CR1_UE; // Enable UART4
When I observed CN5-1 on a scope, no sign of activity.
To debug further, I went to STM32CubeMX and tried to enable UART4 and it was unavailable even though I ensured that no ADC/SDMMC/ETH were enabled. I am using the LCD but it should not conflict. What am I doing wrong?
2020-02-26 8:21 AM
GPIO_InitStruct.Mode = GPIO_MODE_AF_PP;
2020-02-26 8:50 AM
Thanks, but that had no effect. Maybe the answer involves the peculiar CubeMX unavailability of UART4... other USARTs work. BTW, just in case I wasn't clear, my Keil IDE does not object to the code. Also, the code that I pasted above is only a small part of the whole code, so my next step is to delete everything unrelated to UART4... I was hoping that there was a really simple solution.
2020-02-26 11:12 AM
The stripped down version works, so there was some conflict, I guess.