2024-08-15 10:57 PM
Hi,
I use the memory management function to generate a custom ld file, but the generated ld file is wrong.
Solved! Go to Solution.
2024-08-27 03:16 AM
Hello @totoro
After checking, it seems that the issue is related to the MMT with CMake project.
Actually, the Cmake toolchain was added recently in CubeMX, but it currently does not support MMT. The support of MMT with the Cmake project in CubeMX is planned for the next releases.
Thank you for reporting!
KR,
Souhaib
2024-08-16 03:07 AM
Hello @totoro
In order to investigate the issue, could you please provide additional information: the name of MCU the version of CubeMX ...
Thank you,
Souhaib
2024-08-16 08:54 PM
2024-08-27 03:16 AM
Hello @totoro
After checking, it seems that the issue is related to the MMT with CMake project.
Actually, the Cmake toolchain was added recently in CubeMX, but it currently does not support MMT. The support of MMT with the Cmake project in CubeMX is planned for the next releases.
Thank you for reporting!
KR,
Souhaib