cancel
Showing results for 
Search instead for 
Did you mean: 

STM32U5 FreeRTOS MPU Support

BCowp.1
Associate II

Versions:
STM32CubeMX 6.12.0
FreeRTOS X-Cube-FREERTOS 1.1.10 (FreeRTOS Kernel 10.5.1)
STM32U5 MCU Package 1.6.0

Although STM32CubeMX now has support for FreeRTOS, it does not appear to recognise the FreeRTOS support (https://www.freertos.org/Security/04-FreeRTOS-MPU-memory-protection-unit) for the Cortex-M33 MPU: 

BCowp1_1-1724423362897.png

It also does not include mpu_wrappers.c, which means I cannot enable configENABLE_MPU in FreeRTOSConfig.h manually without also copying this from the canonical FreeRTOS kernel release.

I have, in fact, manually imported mpu_wrappers.c and turned on configENABLE_MPU. Everything appears to work quite nicely.

Why is this option not supported?

What, if any, dragons have I unearthed by turning it on?

If the there are no dragons, then clearly this is an oversight and should be included in later releases. It adds a frustrating extra step to upgrading FreeRTOS versions with CubeMX.

 

2 REPLIES 2
Sarra.S
ST Employee

Hello @BCowp.1 , 

Thank you for your feedback 

I've reported this request to the CubeMX team ( Internal Ticket: Ticket 190405). I'll keep you updated if there are any updates 

 

To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.

clemens
Associate II

Hi @Sarra.S , do you have an update on this topic / ticket ?