2021-05-18 1:20 AM
Hello,
I'm using STM32L433RCT-P nucleo board and I was testing some hardware. I noticed the baudrate error with LPUART1 is really high (135100 instead of 115200, 67570 instead of 57600).
I have no problem using manual configuration instead of CubeMX, but, is there a way to obtain the chosen baudrate directly from CubeMX?
Thanks!
MF4
2021-05-18 2:01 AM
In another clean project works better (don't know why because in the other one all i did was sending on lpuart 0x55). Still a bit off though.