cancel
Showing results for 
Search instead for 
Did you mean: 

stm32h7b0vb ADC+dma always Overrun Error

wjun.1
Associate

0693W00000HpnN9QAJ.pngADC Trigger from Timer,DMA transmit ,and then Always Overrun Error, buffer address @0x30000000.Data can not be transferred to buffer correctly,ADC1 register DR is 0x801 while buffer is 0x01.

3 REPLIES 3
TDK
Guru

Show your code. How fast is TIM1? Are you transferring half words or bytes?

If you feel a post has answered your question, please click "Accept as Solution".
Sara BEN HADJ YAHYA
ST Employee

Hello @wjun.1​ ,

Thanks for your feedback,

Could you please specify the CubeMX version and if possible, please share your .ioc file.

Regards,

Sara.

MichaelSweden
Associate III