cancel
Showing results for 
Search instead for 
Did you mean: 

STM32H7 1.9.0 MDMA request not initialized

DShekter
Associate III

Specifically I've noticed it with the octospi, but it's also impacted at least software requests.

For example, my MDMA config has

    hmdma_octospi1_fifo_th.Instance = MDMA_Channel1;
    hmdma_octospi1_fifo_th.Init.TransferTriggerMode = MDMA_BUFFER_TRANSFER;
    hmdma_octospi1_fifo_th.Init.Priority = MDMA_PRIORITY_VERY_HIGH;
    hmdma_octospi1_fifo_th.Init.Endianness = MDMA_LITTLE_ENDIANNESS_PRESERVE;
    hmdma_octospi1_fifo_th.Init.SourceInc = MDMA_SRC_INC_BYTE;
    hmdma_octospi1_fifo_th.Init.DestinationInc = MDMA_DEST_INC_DISABLE;
    hmdma_octospi1_fifo_th.Init.SourceDataSize = MDMA_SRC_DATASIZE_BYTE;
    hmdma_octospi1_fifo_th.Init.DestDataSize = MDMA_DEST_DATASIZE_BYTE;
    hmdma_octospi1_fifo_th.Init.DataAlignment = MDMA_DATAALIGN_RIGHT;
    hmdma_octospi1_fifo_th.Init.BufferTransferLength = 1;
    hmdma_octospi1_fifo_th.Init.SourceBurst = MDMA_SOURCE_BURST_SINGLE;
    hmdma_octospi1_fifo_th.Init.DestBurst = MDMA_DEST_BURST_SINGLE;
    hmdma_octospi1_fifo_th.Init.SourceBlockAddressOffset = 0;
    hmdma_octospi1_fifo_th.Init.DestBlockAddressOffset = 0;
    if (HAL_MDMA_Init(&hmdma_octospi1_fifo_th) != HAL_OK)
    {
      Error_Handler();
    }
 
    __HAL_LINKDMA(ospiHandle,hmdma,hmdma_octospi1_fifo_th);

But what it's missing is the Init.Request. So I had to add

  /* USER CODE BEGIN OCTOSPI1_MspInit 0 */
	  hmdma_octospi1_fifo_th.Init.Request = MDMA_REQUEST_OCTOSPI1_FIFO_TH;
  /* USER CODE END OCTOSPI1_MspInit 0 */

and that fixed everything. a similar thing was needed for the software request, however there are no USER CODE sections in the init function.

Code was generated with the STM32CubeIDE, version 1.7.0.

3 REPLIES 3
Amel NASRI
ST Employee

Hi @Community member​ ,

Thanks for bringing this issue to our attention.

I let our Expert @Khouloud ZEMMELI​ ​ review it and take the required corrective actions, if needed.

-Amel

To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.

Khouloud ZEMMELI
ST Employee

Hello @Community member​ ,

Could you please share your ioc file to check your case?

Thanks, Khouloud

Sure. I've attached an IOC that shows the issue for software and OCTOSPI requests. For me, the initializations look like:

static void MX_MDMA_Init(void)
{
 
  /* MDMA controller clock enable */
  __HAL_RCC_MDMA_CLK_ENABLE();
  /* Local variables */
 
  /* Configure MDMA channel MDMA_Channel0 */
  /* Configure MDMA request hmdma_mdma_channel40_sw_0 on MDMA_Channel0 */
  hmdma_mdma_channel40_sw_0.Instance = MDMA_Channel0;
  hmdma_mdma_channel40_sw_0.Init.TransferTriggerMode = MDMA_BUFFER_TRANSFER;
  hmdma_mdma_channel40_sw_0.Init.Priority = MDMA_PRIORITY_LOW;
  hmdma_mdma_channel40_sw_0.Init.Endianness = MDMA_LITTLE_ENDIANNESS_PRESERVE;
  hmdma_mdma_channel40_sw_0.Init.SourceInc = MDMA_SRC_INC_BYTE;
  hmdma_mdma_channel40_sw_0.Init.DestinationInc = MDMA_DEST_INC_BYTE;
  hmdma_mdma_channel40_sw_0.Init.SourceDataSize = MDMA_SRC_DATASIZE_BYTE;
  hmdma_mdma_channel40_sw_0.Init.DestDataSize = MDMA_DEST_DATASIZE_BYTE;
  hmdma_mdma_channel40_sw_0.Init.DataAlignment = MDMA_DATAALIGN_PACKENABLE;
  hmdma_mdma_channel40_sw_0.Init.BufferTransferLength = 1;
  hmdma_mdma_channel40_sw_0.Init.SourceBurst = MDMA_SOURCE_BURST_SINGLE;
  hmdma_mdma_channel40_sw_0.Init.DestBurst = MDMA_DEST_BURST_SINGLE;
  hmdma_mdma_channel40_sw_0.Init.SourceBlockAddressOffset = 0;
  hmdma_mdma_channel40_sw_0.Init.DestBlockAddressOffset = 0;
  if (HAL_MDMA_Init(&hmdma_mdma_channel40_sw_0) != HAL_OK)
  {
    Error_Handler();
  }
 
  /* MDMA interrupt initialization */
  /* MDMA_IRQn interrupt configuration */
  HAL_NVIC_SetPriority(MDMA_IRQn, 0, 0);
  HAL_NVIC_EnableIRQ(MDMA_IRQn);
 
}

and

/* OCTOSPI1 MDMA Init */
    /* OCTOSPI1_FIFO_TH Init */
    hmdma_octospi1_fifo_th.Instance = MDMA_Channel1;
    hmdma_octospi1_fifo_th.Init.TransferTriggerMode = MDMA_BUFFER_TRANSFER;
    hmdma_octospi1_fifo_th.Init.Priority = MDMA_PRIORITY_LOW;
    hmdma_octospi1_fifo_th.Init.Endianness = MDMA_LITTLE_ENDIANNESS_PRESERVE;
    hmdma_octospi1_fifo_th.Init.SourceInc = MDMA_SRC_INC_BYTE;
    hmdma_octospi1_fifo_th.Init.DestinationInc = MDMA_DEST_INC_BYTE;
    hmdma_octospi1_fifo_th.Init.SourceDataSize = MDMA_SRC_DATASIZE_BYTE;
    hmdma_octospi1_fifo_th.Init.DestDataSize = MDMA_DEST_DATASIZE_BYTE;
    hmdma_octospi1_fifo_th.Init.DataAlignment = MDMA_DATAALIGN_PACKENABLE;
    hmdma_octospi1_fifo_th.Init.BufferTransferLength = 1;
    hmdma_octospi1_fifo_th.Init.SourceBurst = MDMA_SOURCE_BURST_SINGLE;
    hmdma_octospi1_fifo_th.Init.DestBurst = MDMA_DEST_BURST_SINGLE;
    hmdma_octospi1_fifo_th.Init.SourceBlockAddressOffset = 0;
    hmdma_octospi1_fifo_th.Init.DestBlockAddressOffset = 0;
    if (HAL_MDMA_Init(&hmdma_octospi1_fifo_th) != HAL_OK)
    {
      Error_Handler();
    }
 
    __HAL_LINKDMA(hospi,hmdma,hmdma_octospi1_fifo_th);