STM32F411re SPI SDCARD
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2018-03-20 2:57 PM
Hi everybody, I am back here because two weeks ago, I started to try to add a SD card on my nucleo F411re. I used SPI connexion. I tested the wiring with a mbed software called Nucleo_L476RG_SDCard_WorkingSample. I just changed the pin to match my SPI1 on nucleo F411re :
// MOSI, MISO, SCLK, CS, name
SDFileSystem sd(PB_5, PB_4, PB_3, PA_10, 'sd');I tried a lot of things using cubeMX to get this working using SW4STM32. I added FatFS, but since I not using SDIO, CubeMX do not allow to tick SDcard in FatFS. I ticked 'user defined', but after generating the project, I am not able to move forward. I tested every library/tutorial available on the first two pages of a famous web browser. Now I still stucked, with nothing new to try.
Does somebody here could share a project that I could start with ( open it and compile at less using sw4stm32? generated with cubemx ? using Hal? and finaly using a stm32F411?).
Thanks in advance
Baptiste
#stm32f411 #fatfs #sdcard #spi #cubemx #sw4stm32- Labels:
-
FatFS
-
SDIO-SDMMC
-
SPI
-
STM32CubeMX
-
STM32F4 Series
-
SW4STM32
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2018-03-20 3:31 PM
Should be an SPI adafruit example that builds with the nucleo. And fatfs application example under the HAL example trees. On phone will find an example later.
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
‎2018-03-20 7:09 PM
STM32Cube_FW_F4_V1.21.0\Projects\STM32F411RE-Nucleo\Demonstrations\SW4STM32\STM32F4xx_Nucleo\.project
Uses SPI SD Card, and FatFs
STM32Cube_FW_F4_V1.21.0\Drivers\BSP\Adafruit_Shield\stm32_adafruit_sd.c
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
‎2018-03-21 8:40 AM
Hello, thank you for that, that's a good start for me since I can compile for my nucleo. I imported the project into SW4STM32, compiled it, OK . Since I dont use the lcd shield I commented all the lcd related fonctions. I still use spi for my sdcard and I dont find in the project something about spi1, or somewhere to specify witch spi pin I will use...
Could you drive me to the good place to set that?
Thanks a lot
Baptiste
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2018-03-21 9:53 AM
The board specific stuff is defined here
STM32Cube_FW_F4_V1.0\Drivers\BSP\STM32F4xx-Nucleo\stm32f4xx_nucleo.h
STM32Cube_FW_F4_V1.0\Drivers\BSP\STM32F4xx-Nucleo\stm32f4xx_nucleo.c
I'm not using a shield either, I have a spidered up micro sd socket
https://community.st.com/0D50X00009XkYXdSAN
I've used the code as the basis for adding SPI SDCARDs to Nucleo-64 and Nucleo-144 boards.
I personally don't like the SPI implementation because it is very slow, I prefer SDIO or SDMMC as it is significantly more rapid and usable in real-world applications.
Up vote any posts that you find helpful, it shows what's working..