2021-09-25 3:39 PM
I have a blackpill board with STM32F411 48 pins IC and CubeMX/CubeIDE at lastest versions. The USB is configured as device CDC, no Vbus.
When I flash the board with generated code and plug USB in Windows 10 I get an error "invalid device descriptor". I have increased heap to 0x1000 without success.
It not seems a hardware issue because I can enter the board in DFU and flash or erase device using CubeProgrammer.
Any help will be apreciated.
Leonardo
Solved! Go to Solution.
2021-09-26 5:06 AM
I found the solution, I have to increase the heap (0x1000), but this isn't enough to solve. I need to change the automatic clock configs of CubeMX that use internal 16MHz clock as source to core.
The image bellow show the way that works.
2021-09-25 5:49 PM
> It not seems a hardware issue
Then there's an invalid device descriptor. Check with a bus analyzer.
2021-09-26 4:40 AM
But the automatic code generated by CubeMX isn't reliable?
2021-09-26 5:06 AM
I found the solution, I have to increase the heap (0x1000), but this isn't enough to solve. I need to change the automatic clock configs of CubeMX that use internal 16MHz clock as source to core.
The image bellow show the way that works.