User Activity

Could someone help to understand the better value to use at frequency deviation, considering at bellow specs:   #define BASE_FREQUENCY 916000000 //Hz #define MODULATION_SELECT MOD_2GFSK_BT05 #define DATARATE ...
I have a blackpill board with STM32F411 48 pins IC and CubeMX/CubeIDE at lastest versions. The USB is configured as device CDC, no Vbus.​When I flash the board with generated code ​and plug USB in Windows 10 I get an error "invalid device descriptor"...