2021-03-24 12:39 PM
I'm using STM32F103C8T6 controller and I want to connect MAX30003 breakout board. Which preferences it's better to use for the best performance (STMCubeMX)?
Can I communicate it with an SPI slave using the UART1 synchronous mode (configured with CubeMX, using the LL library)??
2023-03-14 6:10 AM
can u please provide code for max30003 if u finished working in that.