2021-05-07 9:01 AM
I configured all pins of stm32f103c8 as output. All pins are toggling and only PD0 and PD1 aren't toggling .. I am using internal crystal of stm32f103c8 then obviously the PD0 and PD1 pins are free for configure as output or input.
Solved! Go to Solution.
2021-05-07 11:27 AM
PD0/PD1 are used by the external oscillator by default. To use them as GPIO pins, see "Using OSC_IN/OSC_OUT pins as GPIO ports PD0/PD1" in the reference manual.
2021-05-07 11:27 AM
PD0/PD1 are used by the external oscillator by default. To use them as GPIO pins, see "Using OSC_IN/OSC_OUT pins as GPIO ports PD0/PD1" in the reference manual.
2021-05-07 10:18 PM
Thank you . Then stm32cube Mx generates faulty code to make remap pins On PD0 and PD1 and configure as IO? Please give me direct solution for this because I am new on stm32
2021-05-07 10:18 PM
Thank you .give me direct solution for this
2021-05-07 10:22 PM
IN REFERENCE MANUAL
9.3.2 Using OSC_IN/OSC_OUT pins as GPIO ports PD0/PD1
The HSE oscillator pins OSC_IN/OSC_OUT can be used as general-purpose I/O PD0/PD1
by programming the PD01_REMAP bit in the AF remap and debug I/O configuration register
(AFIO_MAPR).
This remap is available only on 36-, 48- and 64-pin packages (PD0 and PD1 are available
on 100-pin and 144-pin packages, no need for remapping).
Note: The external interrupt/event function is not remapped. PD0 and PD1 cannot be used for
external interrupt/event generation on 36-, 48- and 64-pin packages.
2021-05-08 12:46 AM
OK so as you have the 48-pin package, you need to set AFIO_MAPR.PD01_REMAP to be able to use the oscillator pins as PD0/PD1. It appers that in Cube/HAL, you could use AFIO_REMAP_ENABLE(AFIO_MAPR_PD01_REMAP) . I don't use Cube.
Note, that to be able to do that, the AFIO clock in RCC has to be enabled first, by setting RCC_APB2ENR.AFIOEN.
JW
2021-05-08 6:06 AM
/**
* @brief GPIO Initialization Function
* @param None
* @retval None
*/
static void MX_GPIO_Init(void)
{
GPIO_InitTypeDef GPIO_InitStruct = {0};
/* GPIO Ports Clock Enable */
__HAL_RCC_GPIOD_CLK_ENABLE();
/*Configure GPIO pin Output Level */
HAL_GPIO_WritePin(GPIOD, GPIO_PIN_0|GPIO_PIN_1, GPIO_PIN_RESET);
/*Configure GPIO pins : PD0 PD1 */
GPIO_InitStruct.Pin = GPIO_PIN_0|GPIO_PIN_1;
GPIO_InitStruct.Mode = GPIO_MODE_OUTPUT_PP;
GPIO_InitStruct.Pull = GPIO_NOPULL;
GPIO_InitStruct.Speed = GPIO_SPEED_FREQ_LOW;
HAL_GPIO_Init(GPIOD, &GPIO_InitStruct);
/*Configure peripheral I/O remapping */
__HAL_AFIO_REMAP_PD01_ENABLE();
}> Then stm32cube Mx generates faulty code to make remap pins
Seems right to me. (Note that __HAL_RCC_AFIO_CLK_ENABLE() is called within HAL_MspInit.)
2021-05-08 7:52 AM
Thank you TDK but not getting Output. Please cheak code
/* MAIN CODE*/
HAL_GPIO_TogglePin(GPIOD,GPIO_PIN_0);
HAL_GPIO_TogglePin(GPIOD,GPIO_PIN_1);
HAL_GPIO_TogglePin(GPIOC,GPIO_PIN_13);
HAL_Delay(10);
/* GPIO INIT FUNCTION*/
static void MX_GPIO_Init(void)
{
GPIO_InitTypeDef GPIO_InitStruct = {0};
/* GPIO Ports Clock Enable */
__HAL_RCC_GPIOC_CLK_ENABLE();
__HAL_RCC_GPIOD_CLK_ENABLE();
__HAL_RCC_GPIOA_CLK_ENABLE();
/*Configure GPIO pin Output Level */
HAL_GPIO_WritePin(GPIOC, GPIO_PIN_13|GPIO_PIN_14|GPIO_PIN_15, GPIO_PIN_RESET);
/*Configure GPIO pin Output Level */
HAL_GPIO_WritePin(GPIOD, GPIO_PIN_0|GPIO_PIN_1, GPIO_PIN_RESET);
/*Configure GPIO pins : PC13 PC14 PC15 */
GPIO_InitStruct.Pin = GPIO_PIN_13|GPIO_PIN_14|GPIO_PIN_15;
GPIO_InitStruct.Mode = GPIO_MODE_OUTPUT_PP;
GPIO_InitStruct.Pull = GPIO_NOPULL;
GPIO_InitStruct.Speed = GPIO_SPEED_FREQ_LOW;
HAL_GPIO_Init(GPIOC, &GPIO_InitStruct);
/*Configure GPIO pins : PD0 PD1 */
GPIO_InitStruct.Pin = GPIO_PIN_0|GPIO_PIN_1;
GPIO_InitStruct.Mode = GPIO_MODE_OUTPUT_PP;
GPIO_InitStruct.Pull = GPIO_NOPULL;
GPIO_InitStruct.Speed = GPIO_SPEED_FREQ_LOW;
HAL_GPIO_Init(GPIOD, &GPIO_InitStruct);
/*Configure peripheral I/O remapping */
__HAL_AFIO_REMAP_PD01_ENABLE();
}
/* SYSTEM INT*/
HAL_StatusTypeDef HAL_Init(void)
{
/* Configure Flash prefetch */
#if (PREFETCH_ENABLE != 0)
#if defined(STM32F101x6) || defined(STM32F101xB) || defined(STM32F101xE) || defined(STM32F101xG) || \
defined(STM32F102x6) || defined(STM32F102xB) || \
defined(STM32F103x6) || defined(STM32F103xB) || defined(STM32F103xE) || defined(STM32F103xG) || \
defined(STM32F105xC) || defined(STM32F107xC)
/* Prefetch buffer is not available on value line devices */
__HAL_FLASH_PREFETCH_BUFFER_ENABLE();
#endif
#endif /* PREFETCH_ENABLE */
/* Set Interrupt Group Priority */
HAL_NVIC_SetPriorityGrouping(NVIC_PRIORITYGROUP_4);
/* Use systick as time base source and configure 1ms tick (default clock after Reset is HSI) */
HAL_InitTick(TICK_INT_PRIORITY);
/* Init the low level hardware */
HAL_MspInit();
/* Return function status */
return HAL_OK;
}
/* MSP INIT */
__weak void HAL_MspInit(void)
{
/* NOTE : This function should not be modified, when the callback is needed,
the HAL_MspInit could be implemented in the user file
*/
}
/*MY EDITED MSP INT*/
__weak void HAL_MspInit(void)
{
/* NOTE : This function should not be modified, when the callback is needed,
the HAL_MspInit could be implemented in the user file
*/
__HAL_RCC_AFIO_CLK_ENABLE();
}
NOT GETTING OUTPUT:confounded_face:
2021-05-08 8:00 AM
Per the comments in the code, you shouldn't modify the HAL_MspInit function. It should be implemented in user code. CubeMX generates it for you within "stm32f1xx_hal_msp.c". Here's what it generated for me:
/**
* Initializes the Global MSP.
*/
void HAL_MspInit(void)
{
/* USER CODE BEGIN MspInit 0 */
/* USER CODE END MspInit 0 */
__HAL_RCC_AFIO_CLK_ENABLE();
__HAL_RCC_PWR_CLK_ENABLE();
/* System interrupt init*/
/** DISABLE: JTAG-DP Disabled and SW-DP Disabled
*/
__HAL_AFIO_REMAP_SWJ_DISABLE();
/* USER CODE BEGIN MspInit 1 */
/* USER CODE END MspInit 1 */
}But that's probably in your code too if you've generated it from CubeMX. If it is, not sure what the issue is. I don't have an F103 board.
2021-05-08 8:02 AM
Thank you .. you tried your best to explain it to me. but my outcomes are zero.as your suggestion i found out
__HAL_AFIO_REMAP_PD01_ENABLE();
__HAL_RCC_AFIO_CLK_ENABLE();
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.