2021-05-07 9:01 AM
I configured all pins of stm32f103c8 as output. All pins are toggling and only PD0 and PD1 aren't toggling .. I am using internal crystal of stm32f103c8 then obviously the PD0 and PD1 pins are free for configure as output or input.
Solved! Go to Solution.
2021-05-08 8:04 AM
#define __HAL_RCC_AFIO_CLK_ENABLE() do { \
__IO uint32_t tmpreg; \
SET_BIT(RCC->APB2ENR, RCC_APB2ENR_AFIOEN);\
/* Delay after an RCC peripheral clock enabling */\
tmpreg = READ_BIT(RCC->APB2ENR, RCC_APB2ENR_AFIOEN);\
UNUSED(tmpreg); \
} while(0U)
2021-05-08 8:23 AM
Thank you friend.. you can try stm32f103c6
Simulation in protues 8.11
2021-05-08 8:31 AM
void HAL_MspInit(void)
{
/* USER CODE BEGIN MspInit 0 */
/* USER CODE END MspInit 0 */
__HAL_RCC_AFIO_CLK_ENABLE();
__HAL_RCC_PWR_CLK_ENABLE();
/* System interrupt init*/
/** NOJTAG: JTAG-DP Disabled and SW-DP Enabled
*/
__HAL_AFIO_REMAP_SWJ_NOJTAG();
/* USER CODE BEGIN MspInit 1 */
/* USER CODE END MspInit 1 */
}
this also generated in my code
2021-05-08 8:32 AM
can you try simulation in protues for me?
protues 8.11 have stm32f103c6 device
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.