STM32F103C8: CubeMX reports conflicts when selecting 3 UARTs plus USB
Options
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
2017-12-17 2:43 PM
Posted on December 17, 2017 at 23:43
I was setting up a project which uses 3 UARTs + USB on a F103.
CubeMX reports a conflict on UART 1 when USB is configured.
I checked the ref man and datasheet but was unable to
see from what this conflict should arise.
There are no shared pins between these IPs.
I also diffed the generated code between variants with USART1
disabled or enabled and did not see obviuos diffs which do not originated
in the fact of wether USARt1 was configured or not.
Is this a false positive on CubeMXes' side?
Thanks.
#usb #cubemx-project #stm32f1-uart
Labels:
- Labels:
-
STM32CubeMX
-
STM32F1 Series
-
USB
0 REPLIES 0