cancel
Showing results for 
Search instead for 
Did you mean: 

STM32CubeMX Version 6.14 Broke SAE Configuration

cvanbeek
Associate III

I just upgraded from version 6.13 to 6.14.  I have an exiting project for an STM32H7B3 that uses SAI1.  When I click the Generate Code button, I get the following warning:

cvanbeek_0-1741289131151.png

(The second warning is also a bug, I'm using CMake on my project so it is irrelevant).

The SAI1 configuration area is also blank and does not show any warnings or errors:

cvanbeek_1-1741289475629.png

If I create a new project for the STM32H7B3LIH6Q, and enable SAI1 SAI A in master mode, my mouse just spins forever and I do not get configuration options.

cvanbeek_2-1741289559363.png

 

0 REPLIES 0