2020-10-14 1:45 PM
STM32CubeMX in version 6.0.1 does generate an invalid alternate function setting for PC8 and TIM3_CH3 for STM32F030C8. The datasheet states that this should be alternate function 0. See https://www.st.com/resource/en/datasheet/stm32f030c8.pdf. A look into the relevant GPIO-STM32F051_gpio_v1_0_Modes.xml file reveals that the signal description for TIM3_CH3 maps to GPIO_AF1_TIM3 instead of GPIO_AF0_TIM3 in case of GPIO pin PC8.
Solved! Go to Solution.
2020-10-22 9:34 AM
Hello @DS.5tarke
I checked for LQFP64 package and I confirm the issue.
I will raise this issue internally for correction.
Thanks for your contribution
Imen
2020-10-22 7:46 AM
Hello,
According to the datasheet, the PC8 is not available for the LQFP48 package.
PC8 is only available for LQFP64 package, as shown in Figure 4 (LQFP64 64-pin package pinout) of datasheet: https://www.st.com/resource/en/datasheet/stm32f030c8.pdf
Imen
2020-10-22 9:34 AM
Hello @DS.5tarke
I checked for LQFP64 package and I confirm the issue.
I will raise this issue internally for correction.
Thanks for your contribution
Imen