cancel
Showing results for 
Search instead for 
Did you mean: 

STM32CubeMX used to configure a CAN channel on stm32f4-discovery

JOsen
Associate III

New to STM32CubeMX. I am using a stm32f4-discovery. I want to use a CAN channel. It seems that the external memory may be blocking me.

Is there a way to get a CAN channel available for this dev board?  

I would like to end up with the LCD + UART + CAN. I hope there is a lighter weight LCD library that will let this happen in the 2MB of STM32 FLASH and avoid the external FLASH.

1 ACCEPTED SOLUTION

Accepted Solutions
JOsen
Associate III

STM32F469I DISCO seems to have a CAN channel that can be configured.

View solution in original post

2 REPLIES 2
JOsen
Associate III

I remembered that I have a STM3210C-Eval available. It has a CAN channel available and configured. I will use that.

This thread can be closed.

JOsen
Associate III

STM32F469I DISCO seems to have a CAN channel that can be configured.