2019-03-11 07:57 PM
New to STM32CubeMX. I am using a stm32f4-discovery. I want to use a CAN channel. It seems that the external memory may be blocking me.
Is there a way to get a CAN channel available for this dev board?
I would like to end up with the LCD + UART + CAN. I hope there is a lighter weight LCD library that will let this happen in the 2MB of STM32 FLASH and avoid the external FLASH.
Solved! Go to Solution.
2020-02-22 08:23 AM
STM32F469I DISCO seems to have a CAN channel that can be configured.
2019-03-17 09:25 AM
I remembered that I have a STM3210C-Eval available. It has a CAN channel available and configured. I will use that.
This thread can be closed.
2020-02-22 08:23 AM
STM32F469I DISCO seems to have a CAN channel that can be configured.