cancel
Showing results for 
Search instead for 
Did you mean: 

STM32CubeMX Generating Code with Licensing Issues

BCarl
Associate

When selecting "Makefile" for Toolchain/IDE with the STM32F4 Family of MCU's, a Linker Script is generated with a license that does not allow the code to be used with anything other than "System Workbench".

**  (c)Copyright Ac6.
**  You may use this file as-is or modify it according to the needs of your
**  project. Distribution of this file (unmodified or modified) is not
**  permitted. Ac6 permit registered System Workbench for MCU users the
**  rights to distribute the assembled, compiled & linked contents of this
**  file as part of an application binary file, provided that it is built
**  using the System Workbench for MCU toolchain.

1 REPLY 1
MNapi
Senior III

I have been using Cube MX for the last month and Keil. Cube MX would generate all the initialization codes for project and open automatically Keil. I have not seen any problems so far.

As far as I know Cube MX is free to download and use.