cancel
Showing results for 
Search instead for 
Did you mean: 

STM32CubeMX don't generate code that enables SYSCFG clock?

Kenny McCormick
Associate
Posted on June 13, 2018 at 17:21

STM32CubeMX: 4.25.1

MCU: stm32f427

In my application, EXTI is used for external signal triggerring. In STM32CubeMX generated codes, MX_GPIO_Init() initializes GPIO & EXTI related stuff but without enabling SYSCFG clock, in which case the EXTI is not functional.

I think as I selected pins as EXTI in GUI of STM32CubeMX, the generator should enable SYSCFG clock automatically otherwise the function of generated code is not complete.

I also noticed that STM32CubeMX 4.26 has been released. I have not tried the lastest version and I don't know if this problem is fixed.

#stm32cubemx #stm32f4 #syscfg-exti #stm32-rcc
This discussion is locked. Please start a new topic to ask your question.
0 REPLIES 0