2024-07-10 6:59 AM
Hi,
after upgrading the whole suite to last release (as 09-jul-2024), code generation breaks code in function MX_FLASH_Init (main.c file).
If without condition is generated at line 19, no indentation on following block (which closes at line 53).
/**
* @brief FLASH Initialization Function
* @PAram None
* @retval None
*/
static void MX_FLASH_Init(void)
{
/* USER CODE BEGIN FLASH_Init 0 */
/* USER CODE END FLASH_Init 0 */
FLASH_OBProgramInitTypeDef pOBInit = {0};
/* USER CODE BEGIN FLASH_Init 1 */
/* USER CODE END FLASH_Init 1 */
HAL_FLASHEx_OBGetConfig(&pOBInit);
if ()
{
if (HAL_FLASH_Unlock() != HAL_OK)
{
Error_Handler();
}
/* Option Bytes settings */
if (HAL_FLASH_OB_Unlock() != HAL_OK)
{
Error_Handler();
}
pOBInit.OptionType = OPTIONBYTE_USER|OPTIONBYTE_BOOTADDR;
pOBInit.USERType = OB_USER_BOR_LEV;
pOBInit.USERConfig = OB_BOR_LEVEL_4;
pOBInit.BootAddrConfig = OB_BOOTADDR_NS0;
pOBInit.BootAddr = 0x08000000;
if (HAL_FLASHEx_OBProgram(&pOBInit) != HAL_OK)
{
Error_Handler();
}
if (HAL_FLASH_OB_Lock() != HAL_OK)
{
Error_Handler();
}
if (HAL_FLASH_Lock() != HAL_OK)
{
Error_Handler();
}
/* Launch Option Bytes Loading */
/*HAL_FLASH_OB_Launch(); */
}
/* USER CODE BEGIN FLASH_Init 2 */
/* USER CODE END FLASH_Init 2 */
}
Attached the IOC file.
Best regards,
Diego
Solved! Go to Solution.
2024-09-18 2:16 AM
2024-07-10 7:47 AM - edited 2024-07-10 8:35 AM
Hello @DMoim.1
I've been able Reproduce this behavior and I've reported to the concerned team for correction ASAP (under internal ticket number 186268). Thank you for reporting the issue.
Best Regards.
STTwo-32
To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
2024-07-12 7:27 AM
Hello @DMoim.1
To temporarily fix this issue , simply activate only the user Configuration (as mentioned below).
It will have the same result of an empty project.
THX
Ghofrane
2024-07-14 11:38 PM
Thanks!
2024-09-18 2:16 AM