2023-11-23 05:00 AM - edited 2023-11-23 06:22 AM
We are pleased to announce you that the official release of STM32CubeMX V6.10.0 is available.
To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
2024-01-22 02:25 AM
Hello @######
I need you to share the STM32CubeMX.log found under .stm32cubemx folder.
Also, originally which version of MX you are using and want to update.
KR,
Semer.
To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
2024-01-22 03:09 AM - edited 2024-01-22 03:09 AM
Hello, whereabouts is the .stm32cubemx folder usually found please? I can't find it in C:/Program files, or in my user documents?
I'm currently using Cube MX 6.4.0 trying to update to 6.10.0 as described previous.
2024-01-22 05:33 AM
Hi,
The log is under the user folder. C:\Users\username\.stm32cubemx
To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
2024-01-22 06:00 AM - edited 2024-01-25 08:53 AM
@Semer CHERNI Please see attached.
2024-01-26 05:39 AM
Hello @######
It seems like you did not start STM32CubeMX as admin the first time after you made the update. As it is necessary to complete the installation process. This is the scenario that made me see the same behavior as yours.
To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
2024-02-02 12:30 AM
Hello, I tried a few times. It finally worked once I stopped adobe acrobat running. Thanks for your help.
2024-02-26 02:41 AM
Is there a timeframe för when to expect the next update to STM32CubeMX?
I keep getting this on a STM32U5A5 project, when I generate code, but I do not see anything wrong with the parameters, and after checking, code generation works again.