2020-04-09 12:49 PM
Hi, I updated everything to the latest CubeMX and packages. When I generate BLE code now (just a simple P2P Server) the build fails because of multiplye defined symbols. Anyone a soluition?
compiling app_ble.c...
../Src/app_ble.c(224): warning: #1296-D: extended constant initialiser used
PLACE_IN_SECTION("TAG_OTA_START") const uint32_t MagicKeywordAddress = (uint32_t)&MagicKeywordValue;
../Src/app_ble.c: 1 warning, 0 errors
linking...
SH_V2_BLE\SH_V2_BLE.axf: Error: L6200E: Symbol OTP_Read multiply defined (by otp_1.o and otp.o).
SH_V2_BLE\SH_V2_BLE.axf: Error: L6200E: Symbol LST_init_head multiply defined (by stm_list_1.o and stm_list.o).
SH_V2_BLE\SH_V2_BLE.axf: Error: L6200E: Symbol LST_insert_tail multiply defined (by stm_list_1.o and stm_list.o).
SH_V2_BLE\SH_V2_BLE.axf: Error: L6200E: Symbol LST_is_empty multiply defined (by stm_list_1.o and stm_list.o).
SH_V2_BLE\SH_V2_BLE.axf: Error: L6200E: Symbol LST_remove_head multiply defined (by stm_list_1.o and stm_list.o).
SH_V2_BLE\SH_V2_BLE.axf: Error: L6200E: Symbol __asm___11_dbg_trace_c_0a3726df____REV16 multiply defined (by dbg_trace_1.o and dbg_trace.o).
SH_V2_BLE\SH_V2_BLE.axf: Error: L6200E: Symbol __asm___11_dbg_trace_c_0a3726df____REVSH multiply defined (by dbg_trace_1.o and dbg_trace.o).
SH_V2_BLE\SH_V2_BLE.axf: Error: L6200E: Symbol __asm___11_dbg_trace_c_0a3726df____RRX multiply defined (by dbg_trace_1.o and dbg_trace.o).
SH_V2_BLE\SH_V2_BLE.axf: Error: L6200E: Symbol DbgTraceBuffer multiply defined (by dbg_trace_1.o and dbg_trace.o).
SH_V2_BLE\SH_V2_BLE.axf: Error: L6200E: Symbol DbgTraceGetFileName multiply defined (by dbg_trace_1.o and dbg_trace.o).
SH_V2_BLE\SH_V2_BLE.axf: Error: L6200E: Symbol DbgTraceInit multiply defined (by dbg_trace_1.o and dbg_trace.o).
SH_V2_BLE\SH_V2_BLE.axf: Error: L6200E: Symbol __asm___5_otp_c_OTP_Read____REV16 multiply defined (by otp_1.o and otp.o).
SH_V2_BLE\SH_V2_BLE.axf: Error: L6200E: Symbol __asm___5_otp_c_OTP_Read____REVSH multiply defined (by otp_1.o and otp.o).
SH_V2_BLE\SH_V2_BLE.axf: Error: L6200E: Symbol __asm___5_otp_c_OTP_Read____RRX multiply defined (by otp_1.o and otp.o).
SH_V2_BLE\SH_V2_BLE.axf: Error: L6200E: Symbol __asm___10_stm_list_c_64162740____REV16 multiply defined (by stm_list_1.o and stm_list.o).
SH_V2_BLE\SH_V2_BLE.axf: Error: L6200E: Symbol __asm___10_stm_list_c_64162740____REVSH multiply defined (by stm_list_1.o and stm_list.o).
SH_V2_BLE\SH_V2_BLE.axf: Error: L6200E: Symbol __asm___10_stm_list_c_64162740____RRX multiply defined (by stm_list_1.o and stm_list.o).
SH_V2_BLE\SH_V2_BLE.axf: Error: L6200E: Symbol LST_get_next_node multiply defined (by stm_list_1.o and stm_list.o).
SH_V2_BLE\SH_V2_BLE.axf: Error: L6200E: Symbol LST_get_prev_node multiply defined (by stm_list_1.o and stm_list.o).
SH_V2_BLE\SH_V2_BLE.axf: Error: L6200E: Symbol LST_get_size multiply defined (by stm_list_1.o and stm_list.o).
SH_V2_BLE\SH_V2_BLE.axf: Error: L6200E: Symbol LST_insert_head multiply defined (by stm_list_1.o and stm_list.o).
SH_V2_BLE\SH_V2_BLE.axf: Error: L6200E: Symbol LST_insert_node_after multiply defined (by stm_list_1.o and stm_list.o).
SH_V2_BLE\SH_V2_BLE.axf: Error: L6200E: Symbol LST_insert_node_before multiply defined (by stm_list_1.o and stm_list.o).
SH_V2_BLE\SH_V2_BLE.axf: Error: L6200E: Symbol LST_remove_node multiply defined (by stm_list_1.o and stm_list.o).
SH_V2_BLE\SH_V2_BLE.axf: Error: L6200E: Symbol LST_remove_tail multiply defined (by stm_list_1.o and stm_list.o).
SH_V2_BLE\SH_V2_BLE.axf: Error: L6200E: Symbol __asm___11_stm_queue_c_ae3b15be____REV16 multiply defined (by stm_queue_1.o and stm_queue.o).
SH_V2_BLE\SH_V2_BLE.axf: Error: L6200E: Symbol __asm___11_stm_queue_c_ae3b15be____REVSH multiply defined (by stm_queue_1.o and stm_queue.o).
SH_V2_BLE\SH_V2_BLE.axf: Error: L6200E: Symbol __asm___11_stm_queue_c_ae3b15be____RRX multiply defined (by stm_queue_1.o and stm_queue.o).
SH_V2_BLE\SH_V2_BLE.axf: Error: L6200E: Symbol CircularQueue_Add multiply defined (by stm_queue_1.o and stm_queue.o).
SH_V2_BLE\SH_V2_BLE.axf: Error: L6200E: Symbol CircularQueue_Empty multiply defined (by stm_queue_1.o and stm_queue.o).
SH_V2_BLE\SH_V2_BLE.axf: Error: L6200E: Symbol CircularQueue_Init multiply defined (by stm_queue_1.o and stm_queue.o).
SH_V2_BLE\SH_V2_BLE.axf: Error: L6200E: Symbol CircularQueue_NbElement multiply defined (by stm_queue_1.o and stm_queue.o).
SH_V2_BLE\SH_V2_BLE.axf: Error: L6200E: Symbol CircularQueue_Remove multiply defined (by stm_queue_1.o and stm_queue.o).
SH_V2_BLE\SH_V2_BLE.axf: Error: L6200E: Symbol CircularQueue_Remove_Copy multiply defined (by stm_queue_1.o and stm_queue.o).
SH_V2_BLE\SH_V2_BLE.axf: Error: L6200E: Symbol CircularQueue_Sense multiply defined (by stm_queue_1.o and stm_queue.o).
SH_V2_BLE\SH_V2_BLE.axf: Error: L6200E: Symbol CircularQueue_Sense_Copy multiply defined (by stm_queue_1.o and stm_queue.o).
Not enough information to list image symbols.
Not enough information to list load addresses in the image map.
Finished: 2 information, 0 warning and 36 error messages.
"SH_V2_BLE\SH_V2_BLE.axf" - 36 Error(s), 1 Warning(s).
Target not created.
Build Time Elapsed: 00:00:05
2020-04-10 1:57 AM
2020-04-10 2:02 AM
2020-04-10 2:08 AM
2020-04-10 2:41 AM
I played around with a few more configurations. I now got the following output:
So it looks like the _1 files generated are causing this. After another build I got the erros back.
Maybe this will can help solve the root cause.
Build started: Project: SH_V2_BLE
*** Using Compiler 'V5.06 update 6 (build 750)', folder: 'C:\Keil_v5\ARM\ARMCC\Bin'
Build target 'SH_V2_BLE'
linking...
SH_V2_BLE\SH_V2_BLE.axf: Warning: L6304W: Duplicate input file sh_v2_ble\dbg_trace_1.o ignored.
SH_V2_BLE\SH_V2_BLE.axf: Warning: L6304W: Duplicate input file sh_v2_ble\otp_1.o ignored.
SH_V2_BLE\SH_V2_BLE.axf: Warning: L6304W: Duplicate input file sh_v2_ble\stm_list_1.o ignored.
SH_V2_BLE\SH_V2_BLE.axf: Warning: L6304W: Duplicate input file sh_v2_ble\stm_queue_1.o ignored.
Program Size: Code=16176 RO-data=972 RW-data=3152 ZI-data=1408
Finished: 0 information, 4 warning and 0 error messages.
FromELF: creating hex file...
"SH_V2_BLE\SH_V2_BLE.axf" - 0 Error(s), 4 Warning(s).
2020-04-10 4:39 AM
Hi,
Thanks for your feedback, issue confirmed, it is raised internally for fix.
Best Regards,
Khouloud.
2020-04-10 6:05 AM
great, thanks!
2020-07-08 2:03 AM
Has there been a solution found for this issue? Im still having this issue with the latest Cube.
Thanks